Android Imx6 Issue - binder: 196:196 transaction failed 29189, size 0-0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android Imx6 Issue - binder: 196:196 transaction failed 29189, size 0-0

Jump to solution
19,813 Views
lakshmikanthr
Contributor III

Hi,

 

I have tried to build the image of android imx6qsabresd. The image was build successful and I have followed  as per instruction given in Android user guide pdf but the thing is when I flash the image in SD CARD and put into sabresd Development board but I was getting error continuously

 

binder: 196:196 transaction failed 29189, size 0-0
binder: 196:196 transaction failed 29189, size 0-0
binder: 196:196 transaction failed 29189, size 0-0
binder: 196:196 transaction failed 29189, size 0-0
binder: 196:196 transaction failed 29189, size 0-0

 

I have also tried with Pre-built image but I was getting same error.

 

May I know why this error was getting. Hope am waiting for your kind reply.

 

 

Thanks & Regards,

R Lakshmikanth

Original Attachment has been moved to: binder-log-error.txt.zip

Labels (1)
0 Kudos
Reply
1 Solution
16,536 Views
lakshmikanthr
Contributor III

Hi,

After modifying the the following bootargs , the binder problem was solved .

U-Boot 2016.03 (Sep 11 2017 - 14:51:40 +0530)

CPU:   Freescale i.MX6Q rev1.2 996 MHz (running at 792 MHz)
CPU:   Automotive temperature grade (-40C to 125C) at 26C
Reset cause: POR
Board: MX6-SabreSD
I2C:   ready
DRAM:  1 GiB
PMIC:  PFUZE100 ID=0x10
MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In:    serial
Out:   serial
Err:   serial
check_and_clean: reg 0, flag_set 0
Fastboot: Normal
flash target is MMC:1
Net:   FEC [PRIME]
Hit any key to stop autoboot:  3     2     0
=> setenv bootargs console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb1:off video=mxcfb2:off vido=mxcfb3:off vmalloc=256M androidboot.console=ttymxc0 consoleblank=0 androidboot.hardware=freescale cma=384M androidboot.selinux=disabled androidboot.dm_verity=disabled
=> saveenv

=> reset

Actually , the kernel system is unable to mount the console path. if you modify the above highlighted command in u-boot , the problem binder issue  was solved. 

Thanks & regards,

R Lakshmikanth

View solution in original post

0 Kudos
Reply
13 Replies
16,535 Views
diegoadrian
NXP Employee
NXP Employee

Hello Lakshmikanth

If you want a quick answer for your problem. You can set the bellow bootargs in the u-boot terminal. Those bootargs, normally solve the binder problem.

U-Boot > setenv bootcmd boota mmc2
U-Boot > setenv bootargs console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,bpp=32
video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off vmalloc=128M androidboot.console=ttymxc0
consoleblank=0 androidboot.hardware=freescale cma=448M androidboot.selinux=permissive
androidboot.dm_verity=disable
U-Boot > saveenv

I hope this can solve your problem.

Best regards,

Diego.

0 Kudos
Reply
16,535 Views
lakshmikanthr
Contributor III

Hi,

Thank you for response.

 I have tried as per your instruction but default bootcmd is fetch from mmc1 but if i modified , it is unable to load the boot and kernel files. It's fails to execute the process.

Hope do u have any idea regrading this.Hope am looking forward for reply.

Thanks & Regards,

R lakshmikanth

0 Kudos
Reply
16,537 Views
lakshmikanthr
Contributor III

Hi,

After modifying the the following bootargs , the binder problem was solved .

U-Boot 2016.03 (Sep 11 2017 - 14:51:40 +0530)

CPU:   Freescale i.MX6Q rev1.2 996 MHz (running at 792 MHz)
CPU:   Automotive temperature grade (-40C to 125C) at 26C
Reset cause: POR
Board: MX6-SabreSD
I2C:   ready
DRAM:  1 GiB
PMIC:  PFUZE100 ID=0x10
MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In:    serial
Out:   serial
Err:   serial
check_and_clean: reg 0, flag_set 0
Fastboot: Normal
flash target is MMC:1
Net:   FEC [PRIME]
Hit any key to stop autoboot:  3     2     0
=> setenv bootargs console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,bpp=32 video=mxcfb1:off video=mxcfb1:off video=mxcfb2:off vido=mxcfb3:off vmalloc=256M androidboot.console=ttymxc0 consoleblank=0 androidboot.hardware=freescale cma=384M androidboot.selinux=disabled androidboot.dm_verity=disabled
=> saveenv

=> reset

Actually , the kernel system is unable to mount the console path. if you modify the above highlighted command in u-boot , the problem binder issue  was solved. 

Thanks & regards,

R Lakshmikanth

0 Kudos
Reply
16,535 Views
lakshmikanthr
Contributor III

Hi,

I have also modify the u-boot 2015 to u-boot 2016 and change the bootargs then binder android issue  problem was solved.

Thanks & Regards,

R lakshmikanth

0 Kudos
Reply
16,535 Views
lakshmikanthr
Contributor III

Hi,

There is no problem of u-boot 2015 or u-boot 2016 .Just modify the bootargs , the android binder issue problem was solved.

Thanks & Regards,

R Lakshmikanth

0 Kudos
Reply
16,530 Views
lakshmikanthr
Contributor III

I have created partition as per instruction given in Android_user_guide.pdf 

where I have attached the sd card partition and flashing the image but I was getting same error binder: 206:206 transaction failed 29189, size 0-0.

Please find the attachments file.

Hope am looking forward for reply.

Thanks & Regards,

R Lakshmikanth

0 Kudos
Reply
16,530 Views
lakshmikanthr
Contributor III

Hi,

Thank you for response.

Please find the attachment of files. Actually one thing I have observed while flashing the all images , I just check out file are contain in the SD card  while opening the sd card , I didn't observe the boot and recovery is unable to mount the device where as cache , vendor,system and data is mounted properly . May be due to this reason it was unable to do the process the things properly.  Hope am looking forward for your reply.

Thanks & Regards,

R, Lakshmikanth

0 Kudos
Reply
16,530 Views
JayTu
NXP Employee
NXP Employee

From your log, you are trying to mount emmc instead of SD card.

Then android can't find necessary command to boot up,

init: error opening block device /dev/block/mmcblk3p2: No such file or directory
init: cannot find '/system/bin/logd', disabling 'logd'
init: cannot find '/system/bin/vold', disabling 'vold'
init: cannot find '/system/bin/tzdatacheck', disabling 'exec 0 (/system/bin/tzdatacheck)'
init: cannot find '/system/bin/logd', disabling 'logd'
init: cannot find '/system/bin/logd', disabling 'logd-reinit'

Make sure you are building bootimage for sd as below,

make bootimage BUILD_TARGET_DEVICE=sd

You can also check vold.fstab to see if it mounts emmc or SD.

0 Kudos
Reply
16,529 Views
lakshmikanthr
Contributor III

Hi,

Thank you for kind reply.

I have tried  as per instruction , make bootimage BUILD_TARGET_DEVICE=sd but I was getting same binder error failed.

Please check the attachment of log file and capture image

Capture.JPG

As per above instruction I have done but I was got same binder failed error. Do you have any idea regrading this.

Hope am waiting for reply.

Thanks & Regards,

Lakshmikanth R

0 Kudos
Reply
16,529 Views
JayTu
NXP Employee
NXP Employee

I can see it mounts some partitions successfully as below, but I still can't see system partition is mounted.

EXT4-fs (mmcblk2p4): Ignoring removed nomblk_io_submit option
EXT4-fs (mmcblk2p4): mounted filesystem with ordered data mode. Opts: nomblk_io_submit,noauto_da_alloc,errors=panic
fs_mgr: __mount(source=/dev/block/mmcblk2p4,target=/data,type=ext4)=0
EXT4-fs (mmcblk2p6): Ignoring removed nomblk_io_submit option
EXT4-fs (mmcblk2p6): mounted filesystem with ordered data mode. Opts: nomblk_io_submit
fs_mgr: __mount(source=/dev/block/mmcblk2p6,target=/cache,type=ext4)=0
EXT4-fs (mmcblk2p7): mounted filesystem with ordered data mode. Opts: (null)
fs_mgr: __mount(source=/dev/block/mmcblk2p7,target=/device,type=ext4)=0

You can try if you can access system partition of SD card on PC.

0 Kudos
Reply
16,529 Views
JayTu
NXP Employee
NXP Employee

And can you also attach your fstab.freescale? It's called root directory under the built out directory.

0 Kudos
Reply
16,529 Views
lakshmikanthr
Contributor III

Hi,

Thank you for response. I have already tried this Avoiding binder issue on android pre-built image - i.MXDev Blog 

but it was not solved the problem. Do you have any idea regrading this one. Hope am awaiting for response.

Thanks & Regards,

R. Lakshmikanth

0 Kudos
Reply
16,529 Views
vanessa_maegima
NXP Employee
NXP Employee
0 Kudos
Reply