Android Boot Time with i.MX 8QuadMax, 8QuadXPlus, 95

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android Boot Time with i.MX 8QuadMax, 8QuadXPlus, 95

1,249 Views
Jack-Cha
Contributor V

Hi iMX-Android Champ !

A customer is reviewing an Android Auto project using the i.MX series.

One of their project requirements is to reach Power On -> Android Home Screen in 15 seconds.
If there is any platform that can approximate 15sec using current Android 14 or later, can you share the boot time information?

If it is more than 15sec to home screen, I would appreciate if you could share any relevant documentation or links so that I can guide them on how to reduce it further.

Thanks.

Best Regards, 

JK

 

Tags (1)
0 Kudos
Reply
3 Replies

1,188 Views
thomas598brown
Contributor I

Hello,
For the i.MX series running Android 14 or later, boot times can vary. However, achieving a boot time of 15 seconds from power-on to the home screen is quite challenging. Typically, boot times are around 20-30 seconds depending on the specific configuration and optimizations.

To help reduce boot time, you can refer to the following resources:

  1. Optimize Boot Times: Android Open Source Project

  2. Boot Time Optimization for i.MX: NXP Community

  3. Android Automotive User's Guide: NXP Semiconductors

These resources provide detailed guidance on optimizing boot times, including tips on reducing logging, using LZ4 compression, and stripping debug symbols.

I hope this helps! Let me know if you need further assistance.


Best regards,
Thomas Brown

0 Kudos
Reply

1,229 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Boot time on i.MX8X & i.MX8QM is ~75Sec for Android Automotive default BSP release, but we do provide as part of the documentation ways to improve this, please refer to the Android Automotive User's Guide chapter 8.9 Boot time tuning
https://www.nxp.com/docs/en/user-guide/Android_Auto_User's_Guide.pdf

Best regards/Saludos,
Aldo.

0 Kudos
Reply

1,163 Views
Jack-Cha
Contributor V

Hi AldoG

So if I try the things introduced in the article to reduce boot time, if the boot time using android auto default image is about 70 seconds, can it be reduced to about 20 seconds by applying the config to improve boot time?
Please provide a convincing estimate before 15-20 seconds to be considered for promotion.

 

Thanks.

Regards, 

Jack

Tags (1)
0 Kudos
Reply