smit@SM1015-LT0262:~/SagarV2/iMXAutomotive/automotive-13.0.0_2.3.0_image_8qmek_car$ sudo ./uuu_imx_android_flash.sh -f imx8qm -a -e -D ./ -t /dev/sdb1
[sudo] password for smit:
This script is validated with uuu 1.4.182 version, it is recommended to align with this version.
dual bootloader is supported
dtbo is supported
dual slot is supported
dynamic parttition is supported
vendor_boot parttition is supported
init_boot parttition is supported
generate lines to flash spl-imx8qm.bin to the partition of bootloader0
generate lines to flash partition-table.img to the partition of gpt
generate lines to flash bootloader-imx8qm.img to the partition of bootloader_a
generate lines to flash dtbo-imx8qm.img to the partition of dtbo_a
generate lines to flash boot.img to the partition of boot_a
generate lines to flash vendor_boot.img to the partition of vendor_boot_a
generate lines to flash init_boot.img to the partition of init_boot_a
generate lines to flash vbmeta-imx8qm.img to the partition of vbmeta_a
generate lines to flash super.img to the partition of super
uuu script generated, start to invoke uuu with the generated uuu script
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.182-0-gda3cd53
Wait for Known USB Device Appear...
Hello @Hassan_Zafirul
Please be sure your board is in serial download mode.
You can check with command in your host machine:
$uuu -lsusb
Best regards,
Salas.