Android 9 not booting in Freescale i.MX6Q

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Android 9 not booting in Freescale i.MX6Q

1,534 次查看
balaarulsankar
Contributor II

Currently I'm working with Freescale i.MX6Q rev1.3 board, trying to boot my board with demo images which NXP provided. But It's not booting from the UART log "init: init first stage started!
init: Using Android DT directory /proc/device-tree/firmware/android/
init: [libfs_mgr]fs_mgr_read_fstab_default(): failed to find device default fstb
init: bool android::init::FirstStageMount::InitRequiredDevices(): partition(s) r
random: fast init done " its halted this stage. Please help me to solve this issue

标签 (1)
2 回复数

1,226 次查看
karangajjar
Senior Contributor II

Hi Arul Sankar,

Kindly refer to below thread:

imx6q sabresd board could not running for android P 

Let us know for any other concern regarding above thread.

Regards,

Karan Gajjar

0 项奖励
回复

1,226 次查看
balaarulsankar
Contributor II

Hi karan gajjar,

Now I'm able to boot my custom board successful after giving right mmc card address in my device tree dtsi file.