Android 9 build error with clean AOSP build

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android 9 build error with clean AOSP build

ソリューションへジャンプ
4,738件の閲覧回数
vinothkumars
Senior Contributor IV

Dear NXP,

 

I am working on IMX8QM with Android 9. I got build error after with clean Android 9 build. 

Build Steps,

     source build/envsetup.sh

     lunch mek_8q_car-userdebug

     make clean 

 

     make -j6

OpenJDK 64-Bit Server VM warning: INFO: os::commit_memory(0x00000000d4400000, 132120576, 0) failed; error='Not enough space' (errno=12)
#
# There is insufficient memory for the Java Runtime Environment to continue.
# Native memory allocation (mmap) failed to map 132120576 bytes for committing reserved memory.

Thanks & Regards,

VinothS,

Regards,
Vinothkumar Sekar
ラベル(2)
0 件の賞賛
返信
1 解決策
4,059件の閲覧回数
vinothkumars
Senior Contributor IV

Build was done. once reboot the system

Thanks & Regards,

VinothS,

Regards,
Vinothkumar Sekar

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
4,060件の閲覧回数
vinothkumars
Senior Contributor IV

Build was done. once reboot the system

Thanks & Regards,

VinothS,

Regards,
Vinothkumar Sekar
0 件の賞賛
返信
4,059件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello VinothS,

The AOSP is supported by Google so I would suggest that you consult the Google Developer Forums.

It seems, however, that you need more RAM (or SWAP) memory for building Android. Please review the requirements from the Android Source repository:

https://source.android.com/setup/build/requirements

I hope this helps.
Regards,

0 件の賞賛
返信
4,058件の閲覧回数
vinothkumars
Senior Contributor IV

Thank you Gusarambula,

Thanks & Regards,

VinothS,

Regards,
Vinothkumar Sekar
0 件の賞賛
返信