Android 6 on imx6 Solo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android 6 on imx6 Solo

4,300件の閲覧回数
vipulkumar
Contributor III

Hi,

I downloaded source code for Android 6 Marshmallow from from the freescale website (Android 6.0.1 Marshmallow (M6.0.1_2.1.0). Now I want to compile it for i.MX6 Solo.

To compile it for i.MX6 Solo, which build name I have to select ?

As per the Android User Guide document (Android_M6.0.1_2.1.1 docs), following are the available build names:

evk_6sl                            i.MX 6SoloLite Evaluation Kit
sabreauto_6q                   i.MX 6Quad/6DualLite/6QuadPlus SABRE-AI Board
sabresd_6dq                   i.MX 6Quad/6DualLite/6QuadPlus SABRE-SD Board and SABRE Platform
sabresd_6sx                   i.MX 6SoloX SABRE-SD Board
sabreauto_6sx                i.MX 6SoloX SABRE-AI Board
sabresd_7d                      i.MX 7Dual SABRE-SD Board

ラベル(4)
0 件の賞賛
返信
1 返信

2,719件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vipul

please refer to Android Frequently Asked Questions document

sect.19 How do I run the image on the i.MX 6Solo board?

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信