Hi,
we have synced and build Android 4.2.3 source (Android_User's_Guide.pdf) for imx6 platform for Sabre SDP hw as per below link documentation.
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMXANDROID&fpsp=1&tab=Documentation_T...
we are facing below error, while Sabre-SDP board is booting with above build .
logcat -
/SensorService( 2756): nuSensorService starting...
I/SurfaceFlinger( 2774): SurfaceFlinger is starting
I/SurfaceFlinger( 2774): SurfaceFlinger's main thread ready to run. Initializing graphics H/W...
D/libEGL ( 2774): loaded /system/lib/egl/libEGL_VIVANTE.so
F/libc ( 2774): Fatal signal 11 (SIGSEGV) at 0x0000000c (code=1), thread 2775 (SurfaceFlinger)
I/DEBUG ( 2344): *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** ***
I/DEBUG ( 2344): Build fingerprint: 'Freescale/sabresd_6dq/sabresd_6dq:4.3/1.0.0-rc2/20131108:eng/dev-keys'
I/DEBUG ( 2344): Revision: '405522'
I/DEBUG ( 2344): pid: 2774, tid: 2775, name: SurfaceFlinger >>> /system/bin/surfaceflinger <<<
I/DEBUG ( 2344): signal 11 (SIGSEGV), code 1 (SEGV_MAPERR), fault addr 0000000c
I/DEBUG ( 2344): r0 00000000 r1 414d183c r2 ffffffdc r3 406b0d80
I/DEBUG ( 2344): r4 00000000 r5 414d1800 r6 000030a0 r7 4022e5cd
I/DEBUG ( 2344): r8 40247750 r9 000000ac sl 401881f4 fp 40247764
I/DEBUG ( 2344): ip 40760eec sp 40624d60 lr 40756373 pc 40649f6e cpsr 000e0030
I/DEBUG ( 2344): d0 0000000000000000 d1 0000000000000000
I/DEBUG ( 2344): d2 0000000000000000 d3 0000000000000000
I/DEBUG ( 2344): d4 0000000000000000 d5 0000000000000000
I/DEBUG ( 2344): d6 0000000000000000 d7 0375028000000000
I/DEBUG ( 2344): d8 0000000000000000 d9 0000000000000000
I/DEBUG ( 2344): d10 0000000000000000 d11 0000000000000000
I/DEBUG ( 2344): d12 0000000000000000 d13 0000000000000000
I/DEBUG ( 2344): d14 0000000000000000 d15 0000000000000000
I/DEBUG ( 2344): d16 418bb40d0aba5e35 d17 3f50624dd2f1a9fc
I/DEBUG ( 2344): d18 41976268f4000000 d19 0000000000000000
I/DEBUG ( 2344): d20 0000000000000000 d21 0000000000000000
I/DEBUG ( 2344): d22 0000000000000000 d23 0000000000000000
I/DEBUG ( 2344): d24 0000000000000000 d25 0000000000000000
I/DEBUG ( 2344): d26 0000000000000000 d27 0000000000000000
I/DEBUG ( 2344): d28 0000000000000000 d29 0000000000000000
I/DEBUG ( 2344): d30 0000000000000000 d31 0000000000000000
I/DEBUG ( 2344): scr 00000010
I/DEBUG ( 2344):
I/DEBUG ( 2344): backtrace:
I/DEBUG ( 2344): #00 pc 00023f6e /system/lib/libGAL.so (gcoHAL_QueryChipCount+9)
I/DEBUG ( 2344): #01 pc 0000236f /system/lib/egl/libEGL_VIVANTE.so
I/DEBUG ( 2344): #02 pc 0000608d /system/lib/egl/libEGL_VIVANTE.so (eglGetProcAddress+12)
I/DEBUG ( 2344): #03 pc 00034385 /system/lib/libEGL.so
I/DEBUG ( 2344): #04 pc 00034477 /system/lib/libEGL.so
I/DEBUG ( 2344): #05 pc 0000e025 /system/lib/libEGL.so
I/DEBUG ( 2344): #06 pc 0000e7ad /system/lib/libEGL.so (eglGetDisplay+24)
I/DEBUG ( 2344): #07 pc 000274bf /system/lib/libsurfaceflinger.so (android::SurfaceFlinger::readyToRun()+38)
I/DEBUG ( 2344): #08 pc 000119ff /system/lib/libutils.so (android::Thread::_threadLoop(void*)+74)
I/DEBUG ( 2344): #09 pc 00011581 /system/lib/libutils.so
I/DEBUG ( 2344): #10 pc 0000ca78 /system/lib/libc.so (__thread_entry+72)
I/DEBUG ( 2344): #11 pc 0000cbf4 /system/lib/libc.so (pthread_create+208)
I/DEBUG ( 2344): #12 pc 00005a14 [heap]
Console log:
init: untracked pid 2281 exited
init: untracked pid 2431 exited
init: untracked pid 2577 exited
init: untracked pid 2580 exited
init: untracked pid 2582 exited
init: untracked pid 2586 exited
init: untracked pid 2591 exited
init: untracked pid 2594 exited
init: untracked pid 2702 exited
init: untracked pid 2721 exited
init: untracked pid 2726 exited
I have also attached logcat.txt file. Please let me know your valuable feedback on above.
Regards
Raj
Original Attachment has been moved to: logcat.txt.zip
This is cause of killing init process. So you might find the root-cause of killing init process, which maybe could be a kernel driver error, in this case the vivante gpu driver, or android hal driver error, library fault, or sometimes android framework error. So There may be many different reasons, one of them is that android init trying to initialize services specified by init.rc failed . I suggest to reinstall the bsp from scratch since, the at first build of the bsp if not common to find this kind of errors.
Hope it helps