Hi,
we have synced and build Android 4.2.3 source (Android_User's_Guide.pdf) for imx6 platform for Sabre SDP hw as per below link documentation.
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMXANDROID&fpsp=1&tab=Documentation_T...
we are facing below error, while Sabre-SDP board is booting with above build .
logcat -
/SensorService( 2756): nuSensorService starting...
I/SurfaceFlinger( 2774): SurfaceFlinger is starting
I/SurfaceFlinger( 2774): SurfaceFlinger's main thread ready to run. Initializing graphics H/W...
D/libEGL ( 2774): loaded /system/lib/egl/libEGL_VIVANTE.so
F/libc ( 2774): Fatal signal 11 (SIGSEGV) at 0x0000000c (code=1), thread 2775 (SurfaceFlinger)
I/DEBUG ( 2344): *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** ***
I/DEBUG ( 2344): Build fingerprint: 'Freescale/sabresd_6dq/sabresd_6dq:4.3/1.0.0-rc2/20131108:eng/dev-keys'
I/DEBUG ( 2344): Revision: '405522'
I/DEBUG ( 2344): pid: 2774, tid: 2775, name: SurfaceFlinger >>> /system/bin/surfaceflinger <<<
I/DEBUG ( 2344): signal 11 (SIGSEGV), code 1 (SEGV_MAPERR), fault addr 0000000c
I/DEBUG ( 2344): r0 00000000 r1 414d183c r2 ffffffdc r3 406b0d80
I/DEBUG ( 2344): r4 00000000 r5 414d1800 r6 000030a0 r7 4022e5cd
I/DEBUG ( 2344): r8 40247750 r9 000000ac sl 401881f4 fp 40247764
I/DEBUG ( 2344): ip 40760eec sp 40624d60 lr 40756373 pc 40649f6e cpsr 000e0030
I/DEBUG ( 2344): d0 0000000000000000 d1 0000000000000000
I/DEBUG ( 2344): d2 0000000000000000 d3 0000000000000000
I/DEBUG ( 2344): d4 0000000000000000 d5 0000000000000000
I/DEBUG ( 2344): d6 0000000000000000 d7 0375028000000000
I/DEBUG ( 2344): d8 0000000000000000 d9 0000000000000000
I/DEBUG ( 2344): d10 0000000000000000 d11 0000000000000000
I/DEBUG ( 2344): d12 0000000000000000 d13 0000000000000000
I/DEBUG ( 2344): d14 0000000000000000 d15 0000000000000000
I/DEBUG ( 2344): d16 418bb40d0aba5e35 d17 3f50624dd2f1a9fc
I/DEBUG ( 2344): d18 41976268f4000000 d19 0000000000000000
I/DEBUG ( 2344): d20 0000000000000000 d21 0000000000000000
I/DEBUG ( 2344): d22 0000000000000000 d23 0000000000000000
I/DEBUG ( 2344): d24 0000000000000000 d25 0000000000000000
I/DEBUG ( 2344): d26 0000000000000000 d27 0000000000000000
I/DEBUG ( 2344): d28 0000000000000000 d29 0000000000000000
I/DEBUG ( 2344): d30 0000000000000000 d31 0000000000000000
I/DEBUG ( 2344): scr 00000010
I/DEBUG ( 2344):
I/DEBUG ( 2344): backtrace:
I/DEBUG ( 2344): #00 pc 00023f6e /system/lib/libGAL.so (gcoHAL_QueryChipCount+9)
I/DEBUG ( 2344): #01 pc 0000236f /system/lib/egl/libEGL_VIVANTE.so
I/DEBUG ( 2344): #02 pc 0000608d /system/lib/egl/libEGL_VIVANTE.so (eglGetProcAddress+12)
I/DEBUG ( 2344): #03 pc 00034385 /system/lib/libEGL.so
I/DEBUG ( 2344): #04 pc 00034477 /system/lib/libEGL.so
I/DEBUG ( 2344): #05 pc 0000e025 /system/lib/libEGL.so
I/DEBUG ( 2344): #06 pc 0000e7ad /system/lib/libEGL.so (eglGetDisplay+24)
I/DEBUG ( 2344): #07 pc 000274bf /system/lib/libsurfaceflinger.so (android::SurfaceFlinger::readyToRun()+38)
I/DEBUG ( 2344): #08 pc 000119ff /system/lib/libutils.so (android::Thread::_threadLoop(void*)+74)
I/DEBUG ( 2344): #09 pc 00011581 /system/lib/libutils.so
I/DEBUG ( 2344): #10 pc 0000ca78 /system/lib/libc.so (__thread_entry+72)
I/DEBUG ( 2344): #11 pc 0000cbf4 /system/lib/libc.so (pthread_create+208)
I/DEBUG ( 2344): #12 pc 00005a14 [heap]
Console log:
init: untracked pid 2281 exited
init: untracked pid 2431 exited
init: untracked pid 2577 exited
init: untracked pid 2580 exited
init: untracked pid 2582 exited
init: untracked pid 2586 exited
init: untracked pid 2591 exited
init: untracked pid 2594 exited
init: untracked pid 2702 exited
init: untracked pid 2721 exited
init: untracked pid 2726 exited
I have also attached logcat.txt file. Please let me know your valuable feedback on above.
Regards
Raj
Original Attachment has been moved to: logcat.txt.zip