Android 4.2.2 images for Freescale i.MX6 SABRE SDP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android 4.2.2 images for Freescale i.MX6 SABRE SDP

1,516 Views
elvisdowson
Contributor I

Hi,

I need to use Android-4.2.2 for a project, but the download links provided here do not work:

i.MX6 D/Q and i.MX6 DL/S Android JB4.2.2_1.0.0-GA release

Would it be possible for me to obtain the demo images, source and document archive for the Android-4.2.2 release for the SABRE SDP?

Thanks!

Regards,

Elvis Dowson

Labels (2)
Tags (1)
0 Kudos
3 Replies

709 Views
SergioSolis
NXP Employee
NXP Employee

Hello Elvis,

Android 4.2.2 is not supported anymore thus not available in our website.

You can currently download 4.4.2 and 4.4.3


Have a great day,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

709 Views
acleung
Contributor I

Hi Sergio,

I'm also looking to get this release package. Is it possible?

Thanks,

Alex

0 Kudos

709 Views
elvisdowson
Contributor I

Hi Sergio,

I just need access to the original distribution. I do not require support for Android-4.2.2, I've worked on it for other platforms.

I really need to use this specific version, and I saw in an earlier thread that a link earlier via a freescale internal sever, for another user who was in the same situation.

Re: Is there any way that I still can get this BSP android_jb4.2.2_1.0.0-ga.tar.gz?

Regards,

Elvis Dowson

0 Kudos