Android 15: Fastboot (cannot upload large files to the board. Sync Abort)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android 15: Fastboot (cannot upload large files to the board. Sync Abort)

267件の閲覧回数
Axent
Contributor III

Hello.
I try to use fastboot for flashing image to the EMMC.
But for some reason the transmission interrupts for super.img (larger than 100 Mb) with error:
"Synchronous Abort" handler, esr 0x96000046"

Axent_0-1752074932699.png

I suppose that this issue could be related fastboot buffer size or something. I don't know.

And in host I see:

Axent_1-1752075065265.png

 


Also the partition table is:
idx 0, ptn 0 name='gpt' start=0 len=2048
idx 1, ptn 0 name='' start=0 len=0
idx 2, ptn 0 name='mcu_os' start=10240 len=512
idx 3, ptn 0 name='all' start=0 len=61071360
idx 4, ptn 0 name='bootloader0' start=0 len=8192
idx 5, ptn 1 name='dtbo_a' start=16384 len=8192
idx 6, ptn 2 name='dtbo_b' start=24576 len=8192
idx 7, ptn 3 name='boot_a' start=32768 len=131072
idx 8, ptn 4 name='boot_b' start=163840 len=131072
idx 9, ptn 5 name='init_boot_a' start=294912 len=16384
idx 10, ptn 6 name='init_boot_b' start=311296 len=16384
idx 11, ptn 7 name='vendor_boot_a' start=327680 len=131072
idx 12, ptn 8 name='vendor_boot_b' start=458752 len=131072
idx 13, ptn 9 name='misc' start=589824 len=8192
idx 14, ptn 10 name='metadata' start=598016 len=524288
idx 15, ptn 11 name='presistdata' start=1122304 len=2048
idx 16, ptn 12 name='super' start=1126400 len=8388608
idx 17, ptn 13 name='userdata' start=9515008 len=49188864
idx 18, ptn 14 name='fbmisc' start=58703872 len=2048
idx 19, ptn 15 name='vbmeta_a' start=58707968 len=2048
idx 20, ptn 16 name='vbmeta_b' start=58712064 len=2048

How can I resolve the problem??

Please, I need help.
Thanks.

0 件の賞賛
返信
1 返信

244件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Abort" handler may be due to memory errors, so for new custom i.MX8M board

recommended first to run ddr test and update image as described in its documentation

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/110...

Regards

 

0 件の賞賛
返信