Android 10 build failure for imx8m-evk

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android 10 build failure for imx8m-evk

5,466件の閲覧回数
jole
Contributor I

I downloaded Android 10 source code and tried to build it for imx8m-evk

Here is my command list for building. 

source build/envsetup.sh
lunch evk_8mq-userdebug
make -j32 2>&1 | tee build-log.txt

But build failed.

Starting ninja...
FAILED: ninja: 'out/target/product/evk_8mq/obj/KERNEL_OBJ/arch/arm64/boot/Image', needed by 'out/target/product/evk_8mq/kernel', missing and no known rule to make it
15:21:47 ninja failed with: exit status 1

タグ(1)
3 返答(返信)

5,068件の閲覧回数
karangajjar
Senior Contributor II

Hi Louis Lee,

Steps have been little changed for latest android version. Please follow below document to build the image:

https://www.nxp.com/docs/en/supporting-information/android_Q10.0.0_1.0.0_docs.zip 

Instead of make -j32 2>&1 | tee build-log.txt, use:
./imx-make.sh -j4 2>&1 | tee build-log.txt

Regards,

Karan Gajjar

5,068件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

did you download source code successfully before build as below?

$ source ~/imx-android-10.0.0_1.0.0/imx_android_setup.sh
$ export MY_ANDROID=~/android_build

0 件の賞賛
返信

5,068件の閲覧回数
le_phuong_nam
Contributor I

Hi Joan Xie,

I can't download source android 10.

It shows: error: RPC failed; curl 56 GnuTLS recv error (-9): A TLS packet with unexpected length was received.
I rebuilt the Git, but it doesn't work

0 件の賞賛
返信