Andriod 5.1.1.2 kernel hangs in IMX 6 SL EVK platform

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Andriod 5.1.1.2 kernel hangs in IMX 6 SL EVK platform

2,165 次查看
lyfsci
Contributor III

Hi  Experts,

The IMX 6 SL EVK Android 5.1.1.2 build freezes after bootup. Then the kernel hangs after some times.

Kindly find the logs below,

PM: suspend entry 1970-01-01 00:01:19.686132634 UTC

PM: Syncing filesystems ... done.

Freezing user space processes ...

PM: Wakeup pending, aborting suspend

last active wakeup source: eventpoll

Freezing of tasks aborted after 0.007 seconds (36 tasks refusing to freeze, wq_busy=0):

Restarting tasks ... done.

PM: suspend exit 1970-01-01 00:01:19.742020884 UTC

PM: suspend entry 1970-01-01 00:01:20.075762301 UTC

PM: Syncing filesystems ... done.

Freezing user space processes ... (elapsed 0.001 seconds) done.

Freezing remaining freezable tasks ... (elapsed 0.001 seconds) done.

Suspending console(s) (use no_console_suspend to debug

标签 (2)
0 项奖励
回复
4 回复数

1,798 次查看
lyfsci
Contributor III

Any answers !!

0 项奖励
回复

1,798 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi lyf sci,

When you use the Demo images running on your board, does it boot up success? Here how do you build the BSP, is any error occur during building?

Have a nice day

Dan

0 项奖励
回复

1,798 次查看
lyfsci
Contributor III

Hi Dan,

Thanks for the reply.

There is no error observed during the compilation process. But when the USB OTG cable remains plugged in then the above issues doesn't comes. Here how to disable the Suspend/resume in the Freescale AOSP ?

Lyf

0 项奖励
回复

1,798 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Lyf,

Sorry for late reply. When the android system boot up, and then go to sleep mode, when you insert other device such as USB flash disk, mouse or keyboard by USB OTG  the system will awake. So here you can go to the setting options on your android system, to set the display time. It will be OK.
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct  button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复