After writen i.MX .sdcard file to SD, SABRE not continue Boot.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

After writen i.MX .sdcard file to SD, SABRE not continue Boot.

1,136 Views
kahjoolee
Contributor II

Hi,

I'm new to embedded programming and would like to boot the i.MX6 Quad SABRE Smart Devices using following steps.

I'm follow the steps guides given by "@Kris Zawada" on the forum.

Here is my screenshot of my steps and the log data from the debug USB port.

I've manage write the <>.sdcard file to the SD card base on command below and the SD size are 16GB. However on the SABRE board, I've not connect the Mouse and the Keyboard on the USB OTG.

ScreenHunter_01 Oct. 17 18.38.jpg

ScreenHunter_02 Oct. 17 18.38.jpg

Here is the log file capture on the USB debug port.

U-Boot 2014.04 (Mar 20 2015 - 23:29:57)

 

CPU:   Freescale i.MX6Q rev1.5 at 792 MHz

CPU:   Temperature 33 C, calibration data: 0x5724cc7d

Reset cause: POR

Board: MX6-SabreSD

I2C:   ready

DRAM:  1 GiB

MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2

*** Warning - bad CRC, using default environment

 

No panel detected: default to Hannstar-XGA

Display: Hannstar-XGA (1024x768)

In:    serial

Out:   serial

Err:   serial

Found PFUZE100 deviceid=10,revid=21

mmc1 is current device

Net:   FEC [PRIME]

Normal Boot

Hit any key to stop autoboot:  0

mmc1 is current device

reading boot.scr

** Unable to read file boot.scr **

reading zImage

** Unable to read file zImage **

Booting from net ...

FEC Waiting for PHY auto negotiation to complete.. done

BOOTP broadcast 1

DHCP client bound to address 192.168.0.119

Using FEC device

TFTP from server 0.0.0.0; our IP address is 192.168.0.119; sending through gateway 192.168.0.1

Filename 'zImage'.

Load address: 0x12000000

Loading: T T T T T T T T T T

Retry count exceeded; starting again

BOOTP broadcast 1

DHCP client bound to address 192.168.0.119

Using FEC device

TFTP from server 0.0.0.0; our IP address is 192.168.0.119; sending through gateway 192.168.0.1

Filename 'zImage'.

Load address: 0x12000000

Loading: T T T T

Labels (1)
3 Replies

874 Views
kahjoolee
Contributor II

Able to run the Yacto Linux on the SABRE board.

874 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Kah Joo Lee,

I'm glad to hear that! Would you mind sharing what went wrong? It may help other community users.

Regards,

0 Kudos

874 Views
kahjoolee
Contributor II

Hi,

Attached was the summary of my step which able to run the Yocto using the .sdcard prebuild file.

My next step was to learn how to change the boot up screen picture to my company logo and learn how to build the Linux and run it on SABRE board.

Then would like to write and simple application on Linux for the project application.

Appreciate if you can lead me where I can learn the steps from begining to advance.

Thanks.

0 Kudos