My environment is:
platform : imx6q
linux kernel: Linux version 3.10.53-88228-g9ebf157-dirty
and I wanted to enlarge the csi0 width from 8 to 16 between my sensor and ipu.
My sensor supports bt656 8-bit and YCbCr 4:2:2 16-bit. Based on IMX6DQRM, the ipu of imx6q supports bt656 8-bit and 16 bit YUV422 (In 37.4.3.9 16-bit camera support.)
Following are my combination:
sensor < --- > imx6
BT656 8-bit BT656 8-bit => fine, please check the attach normal.jpg
YCbCr4:2:2 16-bit IPU_PIX_FMT_GENERIC_16 => wrong, please check the video.mp4
My modifications (I used v4l2 to link my sensor and imx6q):
In my sensor driver:
* ioctl_g_ifparm:
Change the V4L2_IF_TYPE_BT656_SPECIFY to V4L2_IF_TYPE_GATE.
There are detail:
if_type = V4L2_IF_TYPE_GATE;
u.gate.csi_data_width = 9; //16-bit
u.gate.nobt_hs_inv = sensor.HPolarity;
u.gate.nobt_vs_inv = sensor..CurVTiming.VPolarity;
u.gate.latch_clk_inv = 0;
u.gate.swap = 0;
u.gate.frame_start_on_rising_vs = 0;
u.gate.v_sync_correct = 1;
u.gate.clock_curr = sensor.curclk;
u.gate.clock_min = sensor.minclk;
u.gate.clock_max = sensor.maxclk;
* ioctl_g_fmt_cap:
Change the V4L2_PIX_FMT_UYVY to IPU_PIX_FMT_GENERIC_16.
fmt.pix.pixelformat = IPU_PIX_FMT_GENERIC_16;
fmt.pix.width = sensor.HActive;
fmt.pix.height = (sensor.ScanMode != 0) ? sensor.VActive * 2 : sensor.VActive;
fmt.pix.field = V4L2_FIELD_INTERLACED_BT;
fmt.pix.sizeimage = f->fmt.pix.width * f->fmt.pix.height;
fmt.pix.colorspace = V4L2_COLORSPACE_JPEG;
In imx6:
I didn't do any change.
Could someone give me a hand??
Thanks very much!!
Hi!
I have fixed the rolling and 4 frames issues by changing the pixel format to IPU_PIX_FMT_GENERIC_16 of csi->mem channel.
But I got another issue, please see the attachment.
pic_1 is the correct. pic_2 is my current status.
I dump the frame via "mxc-v4l2-capture" program.
Could someone give me a hand??
Thanks very much!!
Yes. I solved this problem two years ago.
765077233@qq.com <admin@community.nxp.com> 於 2019年6月10日 週一 下午10:45寫道:
NXP Community
<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Re: After enable 16 csi0, video is rolling and color was wrong
reply from Kyle Niu
<https://community.nxp.com/people/765077233@qq.com?et=watches.email.thread>
in i.MX Processors - View the full discussion
<https://community.nxp.com/message/1162518?commentID=1162518&et=watches.email.thread#comment-1162518>
Hi Jay
first please verify correct sensor connection, it should be
CSI_DATA19 ~ CSI_DATA4 as shown in Table 66. Camera Input
Signal Cross Reference, Format, and Bits Per Cycle i.MX6DQ Datasheet
http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf
then please try to implement settings suggested in :
MX53 CSI/IDMAC config for Aptina 12-bit grayscale camera?
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi, igorpadykov.
Thanks for your suggestion.
Based on Table 66, I have verified the CSI_DATA19~CSI_DATA4 and the connections are correct with my sensor.
I think I should check the CPMEM.
BTW, I have surveyed some articles like Missing v-sync in Bt.656 capture (rolling video) . I also have the video rolling issue but I make sure that my V_Sync, H_Sync pins are fine by Oscilloscope machine. Do you have any idea??
Thanks again! The information you provide is what I need.