After boot from eMMC,iMX.RT1170 can not read /write eMMC normally.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

After boot from eMMC,iMX.RT1170 can not read /write eMMC normally.

1,581件の閲覧回数
yangaichimantou
Contributor I

Hi,

Our iMX.RT1170 boot from eMMC and firmware run normal.

However in this firmware, we can not initialize the eMMC normally.

We get cmd0,cmd1,cmd2,cmd3,cmd7 response normal.

However when we use cmd8 to read ext csd ,the DATA0 line has no response.

We wonder if the bootRom has changed the eMMC to a special status?

We can read the eMMC if we use other boot mode. Do you have any idea about this problem?

Hope for your reply.

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,560件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @yangaichimantou ,

There should no special setting to eMMC. You can try to reset eMMC and SDHC peripheral again before reinitialize.

 

Regards,

Jing

0 件の賞賛
返信

1,558件の閲覧回数
yangaichimantou
Contributor I

Thank you for your reply.

It proved to be something wrong with the hardware.

0 件の賞賛
返信