After I start CSI, the system is stock.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

After I start CSI, the system is stock.

652 Views
iysheng
Contributor II

I debug ov5640 camera by csi with imx6ull.under rgb565 mode,

The mclk wave as:

687845078.jpg

and the pclk wave as:

446188102.jpg

and the href signal wave as:

260534144.jpg

I wonder are these wave forms right?

And when the dma request bit (BIT12) enabled in CSI_CSICR3 reg. after i start csi , the system get stuck. I put some print code in CSI isr, but nothing can print.

is there something maybe wrong ?

0 Kudos
Reply
1 Reply

623 Views
iysheng
Contributor II

After I use physics address in these registers, the stock problem has solved.

2022-05-18_08-32.png

 

0 Kudos
Reply