Adjusting HDMI_PHY_TXTERM does not change outputs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Adjusting HDMI_PHY_TXTERM does not change outputs

1,154 次查看
chris_hii
Contributor I

We have a design that's facing EMI issues related to the HDMI output and I'd like to try adjusting the drive strength / slew rate on the HDMI lines to see if that helps. From looking at similar issues (381362, 303905), I've tried to follow the guidance in AN4671, but am not able to see a change in the output signals using an oscilloscope on the lines. I'm using memtool and running the commands below to change the TXTERM register. It looks like the TXTERM register is updating properly, but I see no difference in the output signals. Maybe I'm doing something wrong?

EDIT: Copied the corrected commands below.

root@host:~# ./memtool -8 0x123020 8 # check initial register settings
Reading 0x8 count starting at address 0x00123020 0x00123020:  69 19 80 00 00 00 00 08 root@host:~# ./memtool -8 0x123021=0x19; ./memtool -8 0x123023=0x04; ./memtool -8 0x123026=0x10 # write TXTERM Writing 8-bit value 0x19 to address 0x00123021 Writing 8-bit value 0x4 to address 0x00123023 Writing 8-bit value 0x10 to address 0x00123026 root@host:~# ./memtool -8 0x123021=0x19; ./memtool -8 0x123026=0x01 # read TXTERM Writing 8-bit value 0x19 to address 0x00123021 Writing 8-bit value 0x1 to address 0x00123026 root@host:~# ./memtool -8 0x123020 8 Reading 0x8 count starting at address 0x00123020 0x00123020:  69 19 80 04 00 04 00 08
标签 (2)
0 项奖励
回复
1 回复

1,077 次查看
jamesbone
NXP TechSupport
NXP TechSupport

In order to make this change to happen directly in the HDMI module,  it is updating the register configurations in the driver,  compile and update the image, since the OS it is handling the HAL there is no way to update the registers of a module that it is already in use.

The other option that I think can also work, but I have never try it with HDMI, it is to put down the driver, this mean unregister the Module of the HDMI From the Kernel, then modify with Memtool and then register the module back. So this way the kernel owns the change already made.

Hope this helps.

0 项奖励
回复