Adeneo improves the network performance on the iMX6 Windows Embedded Compact (WEC7) solutions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Adeneo improves the network performance on the iMX6 Windows Embedded Compact (WEC7) solutions

1,785 Views
witekio
Contributor III

Adeneo’s expertise in Windows Embedded and i.MX6 is again shown in a new optimized and improved NDIS network driver for the i.MX6 SABRE platforms. The new driver uses optimized send/receive buffer management allowing a significant 72% increase in Tx throughput.


NDIS.PNG


Customers using iMX6 with Windows Embedded solutions can now utilize the high performance NDIS driver allowing them to meet their product performance requirements.


Feel free to comment, subscribe and share :smileywink:

Labels (6)
0 Kudos
Reply
0 Replies