Adeneo improves the network performance on the iMX6 Windows Embedded Compact (WEC7) solutions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Adeneo improves the network performance on the iMX6 Windows Embedded Compact (WEC7) solutions

1,863件の閲覧回数
witekio
Contributor III

Adeneo’s expertise in Windows Embedded and i.MX6 is again shown in a new optimized and improved NDIS network driver for the i.MX6 SABRE platforms. The new driver uses optimized send/receive buffer management allowing a significant 72% increase in Tx throughput.


NDIS.PNG


Customers using iMX6 with Windows Embedded solutions can now utilize the high performance NDIS driver allowing them to meet their product performance requirements.


Feel free to comment, subscribe and share :smileywink:

ラベル(6)
0 件の賞賛
返信
0 返答(返信)