Adeneo Gingerbread for i.MX53 Quick start board repo cannot be fetched

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Adeneo Gingerbread for i.MX53 Quick start board repo cannot be fetched

1,183 Views
RobertBagge
Contributor I

Hi everybody!

I am trying to build Adeneo Gingerbread R.10.4 for i.MX53 Quick start board. I run the following command to get the repo "curl https://dl-ssl.google.com/d1/googlesource/git-repo/repo > ./repo". But when I open the repo file it is a response from the server that no such file can be found there (a 404 error).

Have I missed any step or have the repo been moved? If so, do anyone know the new location of the repo?

0 Kudos
Reply
2 Replies

1,093 Views
RobertBagge
Contributor I

Thank you for the reply. I figured out that the problem was that I was trying to build on Mac OS that uses a case-sensitive file system, which is not eligable for an Android build.

0 Kudos
Reply

1,093 Views
daiane_angolini
NXP Employee
NXP Employee
0 Kudos
Reply