Additional Chip Select lines for SPI interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Additional Chip Select lines for SPI interface

786 次查看
harishs
Contributor I

Hi,

We are developing one of our product using CM-FX6  ( IMX6 Quad based COM form Compulab), is it possible to use available GPIO lines for additional Chip select lines for SPI interface required, the dedicated Chip select lines of SPI are used for some other interfaces in our design.

Regards,

Harish.S

标签 (1)
0 项奖励
回复
1 回复

710 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  It is possible to use available GPIO lines for additional Chip select lines for SPI interface.
But users should control these GPIO lins in software.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复