Adding a Sabre board, i.MX6 SoloX to vehicles

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Adding a Sabre board, i.MX6 SoloX to vehicles

622 Views
paulchen1
Contributor I

Hi, I need to embed a Sabre board into a fleet of vehicles, can I ask a few questions before doing so?

  1. Is there an existing enclosure designed for NXP i.MX6 SoloX board? Can you share the CAD file?
  2. Which version is this board? What is the timeline for future board spin?
  3. Is cooling solution needed to cool this board (assuming 50C ambient temperature)?
  4. Was this board manufactured with production processes, or were manual processes involved?
  5. Any 3D diagrams. We need this to do fit studies to decide on the enclosure.

Thanks for comments

Labels (2)
0 Kudos
2 Replies

543 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Paul,

The SABRE boards are for evaluation and development purposes, they are not intended to be directly used on end-applications.

All the hardware design documentation is included on the following package:

https://www.nxp.com/webapp/Download?colCode=IMX6SOLOX-SABRESDB-DESIGNFILES&appType=license

This board does not have/require cooling for the targeted purpose (evaluation/development).

The part number of the i.MX processor used on this board is the following:

MCIMX6X4EVM10AB (Extended Commercial product, operative from -20 to 105 °C).


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

0 Kudos

543 Views
paulchen1
Contributor I

Hi CarlosCasillas‌ thanks for your reply. Do you have any recommended vendor or industrial designs based on this board? 

0 Kudos