Adding Power-on button on Tep0700-imx6ul

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Adding Power-on button on Tep0700-imx6ul

跳至解决方案
1,750 次查看
caglarabidin
Contributor I

Hi all,

I am using yocto 2.1 krogoth on Tep-0700 imx6ul Technexion panel board. The board does not have power-on button.  I am looking for a way to  assign  one of the gpio pins of the board as a power-on button. How can i make  such a modification  ? I have searched snvs option but  i am not sure whether snvs power-key  can be routed to gpio  or not. Any information would be helpful.

Thanks in advance.

0 项奖励
回复
1 解答
1,066 次查看
igorpadykov
NXP Employee
NXP Employee

Hi caglar

this board uses pf3000 pmic and you will have to add some circuitry for

power-on feature, some example can be found on spf-27392 (p.19) Sabre SD schematic.

Schematics (1)
i.MX6_SABRE_SDP_DESIGNFILES

SABRE Platform for Smart Devices|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,067 次查看
igorpadykov
NXP Employee
NXP Employee

Hi caglar

this board uses pf3000 pmic and you will have to add some circuitry for

power-on feature, some example can be found on spf-27392 (p.19) Sabre SD schematic.

Schematics (1)
i.MX6_SABRE_SDP_DESIGNFILES

SABRE Platform for Smart Devices|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------