Adding NV12 support in imx wayland

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Adding NV12 support in imx wayland

2,268 Views
saseendranathvs
Contributor I

Hi,

I am using imx6qsabreauto board and gstreamer 1.0 to render video.

My requirement is to render NV12 format video through waylandsink. But waylandsink is not able to render NV12 video. At the same time I am able to render NV12 video through imxv4l2sink. . How to enable NV12 support in waylandsink plugin?

I tried forcefully adding NV12 in supported video formats. Then caps negotiation is passed, but I am getting a segmentation fault in wayland-client.so file. 

When I checked with valgrind, It gave the below log

==9243== Process terminating with default action of signal 11 (SIGSEGV)
==9243== Access not within mapped region at address 0x0
==9243== at 0x5BE5EC4: ??? (in /usr/lib/libwayland-client.so.0.3.0)

What is the proper way to add NV12 support for waylandsink? 

0 Kudos
Reply
1 Reply

2,057 Views
igorpadykov
NXP Employee
NXP Employee

Hi Saseendranath

one can look at attached Release Notes sect.6 Multimedia for plugins

developed and supported by nxp. As for waylandsink one can check thread

libimxvpuapi wayland sink issue 

and try to get help from maintainer of gstreamer-imx plugins

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------