Adding HID device support to an i.MX233

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Adding HID device support to an i.MX233

797件の閲覧回数
myke_predko
Senior Contributor III

Gentlebeings,

 

I'm interested in setting up my application as a HID device as well, when it is plugged into a PC.  Could you please provide pointers to either examples or list the steps that you worked through to get a HID device application running?  I am using an i.MX233 with the Linux 2.6.31 Kernel.  This was originally a reply to Wayne on the i.MX233 forum but I thought I would throw it out to the group at large. 

 

I can find examples of creating a Linux HID device like in https://www.kernel.org/doc/Documentation/usb/gadget_hid.txt but they require g_hid.h (as well as other includes & libraries) which are not in the development tools or seemingly created by the ltib options. 

 

Any pointers or idea would be greatly appreciated.


Thanx!


myke

タグ(1)
0 件の賞賛
返信
0 返答(返信)