Hi All,
Currently we are using the iMx8QM EVK with yocto linux running on it.
My query is regarding how to enable the blueZ utility in the same. I added DISTRO_FEATURES_append += "bluez5" in local .conf file but while bitbake command there are compilation error regarding the gstreamer as below-
../../../../git/gst-libs/gst/app/gstappsrc.c: In function 'gst_app_src_class_init':
| ../../../../git/gst-libs/gst/app/gstappsrc.c:290:37: error: 'GST_TYPE_APP_STREAM_TYPE' undeclared (first use in this function)
| "the type of the stream", GST_TYPE_APP_STREAM_TYPE,
| ^~~~~~~~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/app/gstappsrc.c:290:37: note: each undeclared identifier is reported only once for each function it appears in
| ../../../../git/gst-libs/gst/video/navigation.c: In function 'gst_query_list_add_command':
| ../../../../git/gst-libs/gst/video/navigation.c:238:24: error: 'GST_TYPE_NAVIGATION_COMMAND' undeclared (first use in this function)
| g_value_init (&item, GST_TYPE_NAVIGATION_COMMAND);
| ^~~~~~~~~~~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/navigation.c:238:24: note: each undeclared identifier is reported only once for each function it appears in
| ../../../../git/gst-libs/gst/video/video-converter.c: In function 'compute_matrix_to_RGB':
| ../../../../git/gst-libs/gst/video/video-converter.c:820:42: error: 'GST_TYPE_VIDEO_MATRIX_MODE' undeclared (first use in this function)
| GST_VIDEO_CONVERTER_OPT_MATRIX_MODE, GST_TYPE_VIDEO_MATRIX_MODE, DEFAULT_OPT_MATRIX_MODE)
| ^
| ../../../../git/gst-libs/gst/video/video-converter.c:848:31: note: in expansion of macro 'GET_OPT_MATRIX_MODE'
| #define CHECK_MATRIX_NONE(c) (GET_OPT_MATRIX_MODE(c) == GST_VIDEO_MATRIX_MODE_NONE)
| ^~~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c:1406:32: note: in expansion of macro 'CHECK_MATRIX_NONE'
| if (!convert->unpack_rgb && !CHECK_MATRIX_NONE (convert)) {
| ^~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c:820:42: note: each undeclared identifier is reported only once for each function it appears in
| GST_VIDEO_CONVERTER_OPT_MATRIX_MODE, GST_TYPE_VIDEO_MATRIX_MODE, DEFAULT_OPT_MATRIX_MODE)
| ^
| ../../../../git/gst-libs/gst/video/video-converter.c:848:31: note: in expansion of macro 'GET_OPT_MATRIX_MODE'
| #define CHECK_MATRIX_NONE(c) (GET_OPT_MATRIX_MODE(c) == GST_VIDEO_MATRIX_MODE_NONE)
| ^~~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c:1406:32: note: in expansion of macro 'CHECK_MATRIX_NONE'
| if (!convert->unpack_rgb && !CHECK_MATRIX_NONE (convert)) {
| ^~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c: In function 'compute_matrix_to_YUV':
| ../../../../git/gst-libs/gst/video/video-converter.c:820:42: error: 'GST_TYPE_VIDEO_MATRIX_MODE' undeclared (first use in this function)
| GST_VIDEO_CONVERTER_OPT_MATRIX_MODE, GST_TYPE_VIDEO_MATRIX_MODE, DEFAULT_OPT_MATRIX_MODE)
| ^
| ../../../../git/gst-libs/gst/video/video-converter.c:848:31: note: in expansion of macro 'GET_OPT_MATRIX_MODE'
| #define CHECK_MATRIX_NONE(c) (GET_OPT_MATRIX_MODE(c) == GST_VIDEO_MATRIX_MODE_NONE)
| ^~~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c:1424:40: note: in expansion of macro 'CHECK_MATRIX_NONE'
| if (force || (!convert->pack_rgb && !CHECK_MATRIX_NONE (convert))) {
| ^~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c: In function 'chain_convert_to_RGB':
| ../../../../git/gst-libs/gst/video/video-converter.c:822:41: error: 'GST_TYPE_VIDEO_GAMMA_MODE' undeclared (first use in this function)
| GST_VIDEO_CONVERTER_OPT_GAMMA_MODE, GST_TYPE_VIDEO_GAMMA_MODE, DEFAULT_OPT_GAMMA_MODE)
| ^
| ../../../../git/gst-libs/gst/video/video-converter.c:851:31: note: in expansion of macro 'GET_OPT_GAMMA_MODE'
| #define CHECK_GAMMA_REMAP(c) (GET_OPT_GAMMA_MODE(c) == GST_VIDEO_GAMMA_MODE_REMAP)
| ^~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c:1575:14: note: in expansion of macro 'CHECK_GAMMA_REMAP'
| do_gamma = CHECK_GAMMA_REMAP (convert);
| ^~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c: In function 'chain_hscale':
| ../../../../git/gst-libs/gst/video/video-converter.c:828:47: error: 'GST_TYPE_VIDEO_RESAMPLER_METHOD' undeclared (first use in this function)
| GST_VIDEO_CONVERTER_OPT_RESAMPLER_METHOD, GST_TYPE_VIDEO_RESAMPLER_METHOD, \
| ^
| ../../../../git/gst-libs/gst/video/video-converter.c:1618:12: note: in expansion of macro 'GET_OPT_RESAMPLER_METHOD'
| method = GET_OPT_RESAMPLER_METHOD (convert);
| ^~~~~~~~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c: In function 'chain_vscale':
| ../../../../git/gst-libs/gst/video/video-converter.c:828:47: error: 'GST_TYPE_VIDEO_RESAMPLER_METHOD' undeclared (first use in this function)
| GST_VIDEO_CONVERTER_OPT_RESAMPLER_METHOD, GST_TYPE_VIDEO_RESAMPLER_METHOD, \
| ^
| ../../../../git/gst-libs/gst/video/video-converter.c:1650:12: note: in expansion of macro 'GET_OPT_RESAMPLER_METHOD'
| method = GET_OPT_RESAMPLER_METHOD (convert);
| ^~~~~~~~~~~~~~~~~~~~~~~~
| Makefile:873: recipe for target 'libgstvideo_1.0_la-navigation.lo' failed
| make[5]: *** [libgstvideo_1.0_la-navigation.lo] Error 1
| make[5]: *** Waiting for unfinished jobs....
| ../../../../git/gst-libs/gst/tag/tags.c: In function 'gst_tag_image_type_is_valid':
| ../../../../git/gst-libs/gst/video/video-converter.c: In function 'chain_convert':
| ../../../../git/gst-libs/gst/tag/tags.c:235:29: warning: implicit declaration of function 'gst_tag_image_type_get_type' [-Wimplicit-function-declaration]
| klass = g_type_class_ref (gst_tag_image_type_get_type ());
| ^~~~~~~~~~~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/tag/tags.c:235:3: warning: nested extern declaration of 'gst_tag_image_type_get_type' [-Wnested-externs]
| klass = g_type_class_ref (gst_tag_image_type_get_type ());
| ^~~~~
| Makefile:673: recipe for target 'libgstapp_1.0_la-gstappsrc.lo' failed
| make[5]: *** [libgstapp_1.0_la-gstappsrc.lo] Error 1
| make[5]: Leaving directory '/home/airbus/iwg27-release-bsp/build_imx8qm/tmp/work/imx8qm_iwg27m-poky-linux/gstreamer1.0-plugins-base/1.12.2-r0/build/gst-libs/gst/app'
| ../../../../git/gst-libs/gst/video/video-converter.c:820:42: error: 'GST_TYPE_VIDEO_MATRIX_MODE' undeclared (first use in this function)
| GST_VIDEO_CONVERTER_OPT_MATRIX_MODE, GST_TYPE_VIDEO_MATRIX_MODE, DEFAULT_OPT_MATRIX_MODE)
| ^
| ../../../../git/gst-libs/gst/video/video-converter.c:848:31: note: in expansion of macro 'GET_OPT_MATRIX_MODE'
| #define CHECK_MATRIX_NONE(c) (GET_OPT_MATRIX_MODE(c) == GST_VIDEO_MATRIX_MODE_NONE)
| ^~~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c:1727:7: note: in expansion of macro 'CHECK_MATRIX_NONE'
| if (CHECK_MATRIX_NONE (convert)) {
| ^~~~~~~~~~~~~~~~~
| Makefile:561: recipe for target 'all' failed
| make[4]: *** [all] Error 2
| make[4]: Leaving directory '/home/airbus/iwg27-release-bsp/build_imx8qm/tmp/work/imx8qm_iwg27m-poky-linux/gstreamer1.0-plugins-base/1.12.2-r0/build/gst-libs/gst/app'
| ../../../../git/gst-libs/gst/video/video-converter.c:824:45: error: 'GST_TYPE_VIDEO_PRIMARIES_MODE' undeclared (first use in this function)
| GST_VIDEO_CONVERTER_OPT_PRIMARIES_MODE, GST_TYPE_VIDEO_PRIMARIES_MODE, DEFAULT_OPT_PRIMARIES_MODE)
| ^
| ../../../../git/gst-libs/gst/video/video-converter.c:853:34: note: in expansion of macro 'GET_OPT_PRIMARIES_MODE'
| #define CHECK_PRIMARIES_NONE(c) (GET_OPT_PRIMARIES_MODE(c) == GST_VIDEO_PRIMARIES_MODE_NONE)
| ^~~~~~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c:1735:7: note: in expansion of macro 'CHECK_PRIMARIES_NONE'
| if (CHECK_PRIMARIES_NONE (convert)) {
| ^~~~~~~~~~~~~~~~~~~~
| Makefile:837: recipe for target 'app' failed
| make[3]: *** [app] Error 2
| make[3]: *** Waiting for unfinished jobs....
| ../../../../git/gst-libs/gst/video/video-converter.c:822:41: error: 'GST_TYPE_VIDEO_GAMMA_MODE' undeclared (first use in this function)
| GST_VIDEO_CONVERTER_OPT_GAMMA_MODE, GST_TYPE_VIDEO_GAMMA_MODE, DEFAULT_OPT_GAMMA_MODE)
| ^
| ../../../../git/gst-libs/gst/video/video-converter.c:851:31: note: in expansion of macro 'GET_OPT_GAMMA_MODE'
| #define CHECK_GAMMA_REMAP(c) (GET_OPT_GAMMA_MODE(c) == GST_VIDEO_GAMMA_MODE_REMAP)
| ^~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c:1779:14: note: in expansion of macro 'CHECK_GAMMA_REMAP'
| do_gamma = CHECK_GAMMA_REMAP (convert);
| ^~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/tag/tags.c: In function 'gst_tag_image_data_to_image_sample':
| ../../../../git/gst-libs/gst/tag/tags.c:562:23: error: 'GST_TYPE_TAG_IMAGE_TYPE' undeclared (first use in this function)
| "image-type", GST_TYPE_TAG_IMAGE_TYPE, image_type, NULL);
| ^~~~~~~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/tag/tags.c:562:23: note: each undeclared identifier is reported only once for each function it appears in
| ../../../../git/gst-libs/gst/video/video-converter.c: In function 'chain_convert_to_YUV':
| ../../../../git/gst-libs/gst/video/video-converter.c:822:41: error: 'GST_TYPE_VIDEO_GAMMA_MODE' undeclared (first use in this function)
| GST_VIDEO_CONVERTER_OPT_GAMMA_MODE, GST_TYPE_VIDEO_GAMMA_MODE, DEFAULT_OPT_GAMMA_MODE)
| ^
| ../../../../git/gst-libs/gst/video/video-converter.c:851:31: note: in expansion of macro 'GET_OPT_GAMMA_MODE'
| #define CHECK_GAMMA_REMAP(c) (GET_OPT_GAMMA_MODE(c) == GST_VIDEO_GAMMA_MODE_REMAP)
| ^~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c:1935:14: note: in expansion of macro 'CHECK_GAMMA_REMAP'
| do_gamma = CHECK_GAMMA_REMAP (convert);
| ^~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c: In function 'chain_dither':
| ../../../../git/gst-libs/gst/video/video-converter.c:836:44: error: 'GST_TYPE_VIDEO_DITHER_METHOD' undeclared (first use in this function)
| GST_VIDEO_CONVERTER_OPT_DITHER_METHOD, GST_TYPE_VIDEO_DITHER_METHOD, \
| ^
| ../../../../git/gst-libs/gst/video/video-converter.c:1996:12: note: in expansion of macro 'GET_OPT_DITHER_METHOD'
| method = GET_OPT_DITHER_METHOD (convert);
| ^~~~~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c: In function 'convert_get_alpha_mode':
| ../../../../git/gst-libs/gst/video/video-converter.c:816:41: error: 'GST_TYPE_VIDEO_ALPHA_MODE' undeclared (first use in this function)
| GST_VIDEO_CONVERTER_OPT_ALPHA_MODE, GST_TYPE_VIDEO_ALPHA_MODE, DEFAULT_OPT_ALPHA_MODE)
| ^
| ../../../../git/gst-libs/gst/video/video-converter.c:841:30: note: in expansion of macro 'GET_OPT_ALPHA_MODE'
| #define CHECK_ALPHA_COPY(c) (GET_OPT_ALPHA_MODE(c) == GST_VIDEO_ALPHA_MODE_COPY)
| ^~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c:2222:9: note: in expansion of macro 'CHECK_ALPHA_COPY'
| if (CHECK_ALPHA_COPY (convert))
| ^~~~~~~~~~~~~~~~
| Makefile:811: recipe for target 'libgsttag_1.0_la-tags.lo' failed
| make[5]: *** [libgsttag_1.0_la-tags.lo] Error 1
| make[5]: *** Waiting for unfinished jobs....
| ../../../../git/gst-libs/gst/video/video-converter.c: In function 'video_converter_compute_resample':
| ../../../../git/gst-libs/gst/video/video-converter.c:826:42: error: 'GST_TYPE_VIDEO_CHROMA_MODE' undeclared (first use in this function)
| GST_VIDEO_CONVERTER_OPT_CHROMA_MODE, GST_TYPE_VIDEO_CHROMA_MODE, DEFAULT_OPT_CHROMA_MODE)
| ^
| ../../../../git/gst-libs/gst/video/video-converter.c:860:31: note: in expansion of macro 'GET_OPT_CHROMA_MODE'
| #define CHECK_CHROMA_NONE(c) (GET_OPT_CHROMA_MODE(c) == GST_VIDEO_CHROMA_MODE_NONE)
| ^~~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c:2664:7: note: in expansion of macro 'CHECK_CHROMA_NONE'
| if (CHECK_CHROMA_NONE (convert))
| ^~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/tag/gstvorbistag.c: In function 'gst_tag_to_metadata_block_picture':
| ../../../../git/gst-libs/gst/tag/gstvorbistag.c:572:49: error: 'GST_TYPE_TAG_IMAGE_TYPE' undeclared (first use in this function)
| gst_structure_get (mime_struct, "image-type", GST_TYPE_TAG_IMAGE_TYPE,
| ^~~~~~~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/tag/gstvorbistag.c:572:49: note: each undeclared identifier is reported only once for each function it appears in
| Makefile:769: recipe for target 'libgsttag_1.0_la-gstvorbistag.lo' failed
| make[5]: *** [libgsttag_1.0_la-gstvorbistag.lo] Error 1
| make[5]: Leaving directory '/home/airbus/iwg27-release-bsp/build_imx8qm/tmp/work/imx8qm_iwg27m-poky-linux/gstreamer1.0-plugins-base/1.12.2-r0/build/gst-libs/gst/tag'
| Makefile:636: recipe for target 'all' failed
| make[4]: *** [all] Error 2
| make[4]: Leaving directory '/home/airbus/iwg27-release-bsp/build_imx8qm/tmp/work/imx8qm_iwg27m-poky-linux/gstreamer1.0-plugins-base/1.12.2-r0/build/gst-libs/gst/tag'
| Makefile:837: recipe for target 'tag' failed
| make[3]: *** [tag] Error 2
| ../../../../git/gst-libs/gst/video/video-converter.c: In function 'get_scale_format':
| ../../../../git/gst-libs/gst/video/video-converter.c:5794:3: warning: enumeration value 'GST_VIDEO_FORMAT_NV12_10LE' not handled in switch [-Wswitch]
| switch (format) {
| ^~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c: In function 'setup_scale':
| ../../../../git/gst-libs/gst/video/video-converter.c:828:47: error: 'GST_TYPE_VIDEO_RESAMPLER_METHOD' undeclared (first use in this function)
| GST_VIDEO_CONVERTER_OPT_RESAMPLER_METHOD, GST_TYPE_VIDEO_RESAMPLER_METHOD, \
| ^
| ../../../../git/gst-libs/gst/video/video-converter.c:5923:12: note: in expansion of macro 'GET_OPT_RESAMPLER_METHOD'
| method = GET_OPT_RESAMPLER_METHOD (convert);
| ^~~~~~~~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c: In function 'video_converter_lookup_fastpath':
| ../../../../git/gst-libs/gst/video/video-converter.c:822:41: error: 'GST_TYPE_VIDEO_GAMMA_MODE' undeclared (first use in this function)
| GST_VIDEO_CONVERTER_OPT_GAMMA_MODE, GST_TYPE_VIDEO_GAMMA_MODE, DEFAULT_OPT_GAMMA_MODE)
| ^
| ../../../../git/gst-libs/gst/video/video-converter.c:851:31: note: in expansion of macro 'GET_OPT_GAMMA_MODE'
| #define CHECK_GAMMA_REMAP(c) (GET_OPT_GAMMA_MODE(c) == GST_VIDEO_GAMMA_MODE_REMAP)
| ^~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c:6650:7: note: in expansion of macro 'CHECK_GAMMA_REMAP'
| if (CHECK_GAMMA_REMAP (convert) && (!same_size || in_transf != out_transf))
| ^~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c:820:42: error: 'GST_TYPE_VIDEO_MATRIX_MODE' undeclared (first use in this function)
| GST_VIDEO_CONVERTER_OPT_MATRIX_MODE, GST_TYPE_VIDEO_MATRIX_MODE, DEFAULT_OPT_MATRIX_MODE)
| ^
| ../../../../git/gst-libs/gst/video/video-converter.c:848:31: note: in expansion of macro 'GET_OPT_MATRIX_MODE'
| #define CHECK_MATRIX_NONE(c) (GET_OPT_MATRIX_MODE(c) == GST_VIDEO_MATRIX_MODE_NONE)
| ^~~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c:6661:7: note: in expansion of macro 'CHECK_MATRIX_NONE'
| if (CHECK_MATRIX_NONE (convert)) {
| ^~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c:824:45: error: 'GST_TYPE_VIDEO_PRIMARIES_MODE' undeclared (first use in this function)
| GST_VIDEO_CONVERTER_OPT_PRIMARIES_MODE, GST_TYPE_VIDEO_PRIMARIES_MODE, DEFAULT_OPT_PRIMARIES_MODE)
| ^
| ../../../../git/gst-libs/gst/video/video-converter.c:853:34: note: in expansion of macro 'GET_OPT_PRIMARIES_MODE'
| #define CHECK_PRIMARIES_NONE(c) (GET_OPT_PRIMARIES_MODE(c) == GST_VIDEO_PRIMARIES_MODE_NONE)
| ^~~~~~~~~~~~~~~~~~~~~~
| ../../../../git/gst-libs/gst/video/video-converter.c:6671:7: note: in expansion of macro 'CHECK_PRIMARIES_NONE'
| if (CHECK_PRIMARIES_NONE (convert)) {
| ^~~~~~~~~~~~~~~~~~~~
| Makefile:915: recipe for target 'libgstvideo_1.0_la-video-converter.lo' failed
| make[5]: *** [libgstvideo_1.0_la-video-converter.lo] Error 1
| make[5]: Leaving directory '/home/airbus/iwg27-release-bsp/build_imx8qm/tmp/work/imx8qm_iwg27m-poky-linux/gstreamer1.0-plugins-base/1.12.2-r0/build/gst-libs/gst/video'
| Makefile:715: recipe for target 'all' failed
| make[4]: *** [all] Error 2
| make[4]: Leaving directory '/home/airbus/iwg27-release-bsp/build_imx8qm/tmp/work/imx8qm_iwg27m-poky-linux/gstreamer1.0-plugins-base/1.12.2-r0/build/gst-libs/gst/video'
| ERROR: oe_runmake failed
| Makefile:837: recipe for target 'video' failed
| make[3]: *** [video] Error 2
| make[3]: Leaving directory '/home/airbus/iwg27-release-bsp/build_imx8qm/tmp/work/imx8qm_iwg27m-poky-linux/gstreamer1.0-plugins-base/1.12.2-r0/build/gst-libs/gst'
| Makefile:534: recipe for target 'all-recursive' failed
| make[2]: *** [all-recursive] Error 1
| make[2]: Leaving directory '/home/airbus/iwg27-release-bsp/build_imx8qm/tmp/work/imx8qm_iwg27m-poky-linux/gstreamer1.0-plugins-base/1.12.2-r0/build/gst-libs'
| Makefile:673: recipe for target 'all-recursive' failed
| make[1]: *** [all-recursive] Error 1
| make[1]: Leaving directory '/home/airbus/iwg27-release-bsp/build_imx8qm/tmp/work/imx8qm_iwg27m-poky-linux/gstreamer1.0-plugins-base/1.12.2-r0/build'
| Makefile:604: recipe for target 'all' failed
| make: *** [all] Error 2
| ERROR: Function failed: do_compile (log file is located at /home/airbus/iwg27-release-bsp/build_imx8qm/tmp/work/imx8qm_iwg27m-poky-linux/gstreamer1.0-plugins-base/1.12.2-r0/temp/log.do_compile.22664)
ERROR: Task (/home/airbus/iwg27-release-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-multimedia/gstreamer/gstreamer1.0-plugins-base_1.12.2.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 3220 tasks of which 3219 didn't need to be rerun and 1 failed.
Summary: 1 task failed:
/home/airbus/iwg27-release-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-multimedia/gstreamer/gstreamer1.0-plugins-base_1.12.2.bb:do_compile
Summary: There were 3 WARNING messages shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.
Request you all to please suggest, how can I solve this issue or any other way to add blueZ utility to yocto linux.
Thanks & Regards,
Ratnakar
Hello,
Unfortunately, we cannot help you with that, since the i.MX8QM is not officialy released yet and we do not have a way to test your problem. I apologize for the inconveniences this could give you.
Best Regards,
Diego