I'm trying to add imx-gpu-viv recipes into my image but I have some error
After some resarch my problem seems to come of the the variable MACHINEOVERRIDES =. "use-${IMX_DEFAULT_BSP}-bsp:" not present in previous imx-base.inc file of meta-freescale
on an old environnement the command 'bitbake -e | grep MACHINEOVERRIDES=" return
MACHINEOVERRIDES="armv7a:imx:mx6:imxipu:imxvpu:imxgpu2d:imxgpu3d:mx6q:imx6q-apm4"
on Dunfell I've get
MACHINEOVERRIDES="armv7a:use-mainline-bsp:imx6q-apm4"
Hox to fix the problem ?
Thanks
Regards
Solved! Go to Solution.
>When you write "NXP does not have Dunfell do you mean that NXP does not
>support Dunfell LTS linux distribution ?
yes. Supported versions for each nxp bsp can be found in sect.2.1 New features Release Notes
document available on
Best regards
igor
Hi Igor
When you write "NXP does not have Dunfell do you mean that NXP does not support Dunfell LTS linux distribution ?
Otherwise, to fix previous problem, i set IMX_DEFAULT_BSP to "nxp" but I meet some problem with REFERRED_PROVIDER_virtual/libgl defenition as below
ERROR: Nothing PROVIDES 'virtual/libgl' (but /home/dev/MaMachine/tmp_yocto/sources/poky/meta/recipes-graphics/libsdl2/libsdl2_2.0.12.bb DEPENDS on or otherwise requires it)
mesa-gl PROVIDES virtual/libgl but was skipped: PREFERRED_PROVIDER_virtual/libgl set to imx-gpu-viv, not mesa-gl
I've post this message on NXP because I've set IMX_DEFAULT_BSP to "nxp"
Regards
Serge
>When you write "NXP does not have Dunfell do you mean that NXP does not
>support Dunfell LTS linux distribution ?
yes. Supported versions for each nxp bsp can be found in sect.2.1 New features Release Notes
document available on
Best regards
igor
Hi Serge
nxp does not have dunfell. One can try with nxp linux releases described on
For dunfell issues may be recommended to post issue on meta-fsl-arm mailing list:
https://lists.yoctoproject.org/g/meta-freescale
Best regards
igor