Add new lvds with clock frequency 25.18mHz

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Add new lvds with clock frequency 25.18mHz

2,141件の閲覧回数
giorgiofantin
Contributor I

Hi to everybody,

  i coming crazy to add a new lvds to my embedded linux. I have an i.MX6 with kernel versoin 3.0.35 and FS ubuntu 12.02.

It works fine, but now i have to add a new lvds with a resolution as 640 x 480. Its clock frequency is about 25.18 with a maximum of 28.33. I added in ldc.c the new resolution, but with default valued i get a clock frequency of 38 MHz. Searching on google, i found to modifify clock.c file (arch/arm/mach-mx6/clock.c) and set

clk_set_parent(&ldb_di0_clk, &pll5_video_main_clk);

Defautl value is clk_set_parent(&ldb_di0_clk, &pll2_pfd_352M);

Chanching it, the clock frequency goes from 38kHz to 33, but not to 25.

Can anyone help me?

Thnaks

ラベル(2)
タグ(3)
0 件の賞賛
返信
4 返答(返信)

1,702件の閲覧回数
giorgiofantin
Contributor I

i foget to add the declare in ldb.c

Here it is:

{

     "LDB-VGA2B", 60, 640, 480, 30060, //, // Rif. 640x480 BIG DISPLAY LVDS

     40, 40,

     22, 23,

     96, 1,  

     0,

     FB_VMODE_NONINTERLACED,

     FB_MODE_IS_DETAILED,},

Any help?

Thanks

0 件の賞賛
返信

1,702件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Giorgio,

Perhaps the following Community Thread may be of help

https://community.freescale.com/message/331739


Please keep in mind that the clock configuration may not allow for all desired values to be reached so perhaps you wont' be able to get to 25.18Mhz.

0 件の賞賛
返信

1,702件の閲覧回数
giorgiofantin
Contributor I

Hi Gusarambula,

  thanks for the answer, but i followed that guide and nothing goes on the right way.

in any case, the image on display is showed, but not centered perfectly on the screen....

I don't understand if this missmatch is a problem of frequency or a problem of horizontal sync

0 件の賞賛
返信

1,702件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Giorgio,

If  the image is shown correctly but not centered I would recommend looking at the horizontal sync first. Have you had success on your application?

0 件の賞賛
返信