Add i2c touchscreen on DTS file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Add i2c touchscreen on DTS file

3,596件の閲覧回数
mauriciokarrei
Contributor II

Hi,

I need to add a touchscreen driver on my i.mx6. I'm using Yocto and the kernel version is 3.10.

My touchscreen works with i2c communication and I'm tryng to add the parameters in my dts file (imx6q-qmx6.dts), but I'm with some doubts on the configurations. I don't know if the way of declare the variables is correct. The irq e rst pins can be declared with the GPIO number or I need to use another way?

See below the code that I added on dts file.

i2c@3 {

  clock-frequency = <400000>;

  tsc@24 {

  compatible = "cy,cyttsp5_i2c_adapter";

  reg = <0x24>;

  /* GPIO 38, high-to-low edge triggered */

  interrupts = <6 2>;

  interrupt-parent = <&gpio2>;

  cy,adapter_id = "cyttsp5_i2c_adapter";

  cy,core {

  cy,name = "cyttsp5_core";

  cy,id = "main_ttsp_core";

  cy,irq_gpio = <&gpio6>;

  cy,rst_gpio = <&gpio4>;

  cy,hid_desc_register = <1>;

  /* CY_CORE_FLAG_WAKE_ON_GESTURE */

  cy,flags = <1>;

  cy,mt {

  cy,name = "cyttsp5_mt";

  cy,inp_dev_name = "cyttsp5_mt";

  /* CY_MT_FLAG_FLIP | CY_MT_FLAG_INV_X | CY_MT_FLAG_INV_Y */

  cy,flags = <0x38>;

  cy,abs =

  /* ABS_MT_POSITION_X, CY_ABS_MIN_X, CY_ABS_MAX_X, 0, 0 */

  <0x35 0 880 0 0

  /* ABS_MT_POSITION_Y, CY_ABS_MIN_Y, CY_ABS_MAX_Y, 0, 0 */

  0x36 0 1280 0 0

  /* ABS_MT_PRESSURE, CY_ABS_MIN_P, CY_ABS_MAX_P, 0, 0 */

  0x3a 0 255 0 0

  /* CY_IGNORE_VALUE, CY_ABS_MIN_W, CY_ABS_MAX_W, 0, 0 */

  0xffff 0 255 0 0

  /* ABS_MT_TRACKING_ID, CY_ABS_MIN_T, CY_ABS_MAX_T, 0, 0 */

  0x39 0 15 0 0

  /* ABS_MT_TOUCH_MAJOR, 0, 255, 0, 0 */

  0x30 0 255 0 0

  /* ABS_MT_TOUCH_MINOR, 0, 255, 0, 0 */

  0x31 0 255 0 0

  /* ABS_MT_ORIENTATION, -128, 127, 0, 0 */

  0x34 0xfffffed7 127 0 0

  /* ABS_MT_TOOL_TYPE, 0, MT_TOOL_MAX, 0, 0 */

  0x37 0 1 0 0>;

  };

  cy,btn {

  cy,name = "cyttsp5_btn";

  cy,inp_dev_name = "cyttsp5_btn";

  };

  cy,proximity {

  cy,name = "cyttsp5_proximity";

  cy,inp_dev_name = "cyttsp5_proximity";

  cy,abs =

  /* ABS_DISTANCE, CY_PROXIMITY_MIN_VAL, CY_PROXIMITY_MAX_VAL, 0, 0 */

  <0x19 0 1 0 0>;

  };

  };

  };

Thanks

ラベル(2)
0 件の賞賛
返信
1 返信

2,129件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Mauricio

one can look at example of sabresd egalax touchscreen :

egalax_ts, i2c2

linux-2.6-imx.git - Freescale i.MX Linux Tree

linux-2.6-imx.git - Freescale i.MX Linux Tree

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信