Add DDR4 memory up to 8GB on imx8mp

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Add DDR4 memory up to 8GB on imx8mp

2,898件の閲覧回数
xjy198903
Contributor IV

I have a self-made imx8mp motherboard, the model using DDR4 is: K4ABG165WA-MCWE, the single chip capacity is 32Gb, the main frequency is 3200Mhz, my motherboard uses two chips, but the configuration cannot be completed using MX8M_Plus_DDR4_RPA_v9.xlsx

0 件の賞賛
返信
6 返答(返信)

2,884件の閲覧回数
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @xjy198903,

I hope you are doing well.

Could you please send your RPA file for review?

Thanks & Regards,
Ritesh M Patel

0 件の賞賛
返信

2,879件の閲覧回数
xjy198903
Contributor IV

register_config.png
when the clock cycle freq is setting 3200,the ddr stress test file :

xjy198903_0-1683798945817.png

In summary, this tool cannot complete the configuration of Samsung K4ABG165WA MCWE in IMX8MP (DDR, non lpddr)

0 件の賞賛
返信

2,848件の閲覧回数
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @xjy198903,

Please share the schematic of the processor and DRAM interface for review.

Also, 3200 is the data rate. The cycle clock frequency will be 1600MHz.

Thanks & Regards,
Ritesh M Patel

0 件の賞賛
返信

2,845件の閲覧回数
xjy198903
Contributor IV

According to the chip manual, I changed the configuration strategy, RSA can meet my needs: 

xjy198903_0-1683884798035.png

 

0 件の賞賛
返信

2,842件の閲覧回数
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @xjy198903,

Good to hear that it is working now.

Thanks & Regards,
Ritesh M Patel

0 件の賞賛
返信

2,878件の閲覧回数
xjy198903
Contributor IV

the "DDR4 Density per Device (Gb)" can not input 32

0 件の賞賛
返信