Hi All,
I am trying to use airtel 4g dongle in imx6 sabresd as serial modem, for that using usb modeswitch i am converting from cd rom to serial device such that i got /dev/ttyUSB0 node. so further what i should do to use it as a serial modem and i want to ping google- ping 8.8.8.8. If any one knows please help me.
Thanks &Regards,
Lavnaya
Hi all,
I reached in this up to getting /dev/ttyUSB0
i am using screen or minicom to pass the AT commands
AT
OK
ATZ
OK
ATQ0
OK
AT+CPIN?
ERROR
AT+CPIN=?
ERROR
ATI
Manufacturer: huawei
Model: E5573s-606
Revision: 21.315.01.01.284
IMEI: 866079021892317
+GCAP: +CGSM,+DS,+ES
OK
why it is giving error but this device is working as cdc_ether fine and i can able to access network also.
AT+COPS?
ERROR
AT+CQS?
ERROR
AT+CGMI
huawei
OK
AT+CGMm
E5573s-606
OK
AT+CGREG?
ERROR
AT+CGATT?
ERROR
If we check here only device details i can able to get, but i am not able to control it, If any one knows kindly help me .
Thanks
Lavanya
Hi Lavnaya
one can check usb modem linux integration guide from huawei,
in general integration steps should be provided by modem vendor
http://consumer.huawei.com/en/solutions/m2m-solutions/products/support/application-guides/detail/mu6...
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov,
Thanks for information, i gone through that document, as of now i am checking in Linux PC 14.04 and 12.04 ubuntu versions.
I am getting only /dev/ttyUSB0 but in document they given /dev/ttyUSB1 and /dev/ttyUSB2 also but any have they mentioned /dev/ttyUSB0 is for AT commands. But as i mentioned above only device details i can able to get.
Thanks & Regards,
Lavanya
probably may be useful cellular module usage on:
https://boundarydevices.com/product/mu609/
Best regards
igor
Hi igorpadykov,
Sorry i am not able to get what you are trying to explain, Can you please explain me in detail, i am new for this.
Thanks & Regards,
Lavanya
provided link explains usb dongle usage in ubuntu
Cellular modems on i.MX6 boards under Ubuntu - Boundary Devices
Best regards
igor