HELP! anywhere I can download an image for the demo SD card that has linux and Android?
I have the i.MX6Quad SABRE SD Platform
the SD card had Android OS installed.
Tried to follow these guides to get the linux kernel to boot but nothing happens when powered on, no output from serial.
u-boot on the i.MX6 sabre sd platform in a few commands
Linux on the i.MX6 sabre sd platform in a few commands
any advice is greatly appreciated.
解決済! 解決策の投稿を見る。
Hi,
You could download the Android and Linux demo images for regenerating the SD cards using Linux dd command or the MFGtool on Windows. Please refer to the “DEMO_BSPs” downloadable from “Operating System Software-Board Support Packages” section of the following link:
SABRE for Smart Devices Reference Design|Freescale
You could use the Linux dd command in the following way:
$ sudo dd if=<image name>.sdcard of=/dev/sd<partition> bs=1M && sync
For more information, you could refer to section 6.1 “Flashing an SD card image” of “Freescale Yocto Project User's Guide” document. For the MFGtool usage, please refer to section 4.2.2 “Using MFGTool” of “i.MX Linux User's Guide” document.
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
You could download the Android and Linux demo images for regenerating the SD cards using Linux dd command or the MFGtool on Windows. Please refer to the “DEMO_BSPs” downloadable from “Operating System Software-Board Support Packages” section of the following link:
SABRE for Smart Devices Reference Design|Freescale
You could use the Linux dd command in the following way:
$ sudo dd if=<image name>.sdcard of=/dev/sd<partition> bs=1M && sync
For more information, you could refer to section 6.1 “Flashing an SD card image” of “Freescale Yocto Project User's Guide” document. For the MFGtool usage, please refer to section 4.2.2 “Using MFGTool” of “i.MX Linux User's Guide” document.
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you, Carlos!