Accessing SDIO pins in MCIMX28EVKJ: i.MX28 Evaluation Kit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Accessing SDIO pins in MCIMX28EVKJ: i.MX28 Evaluation Kit

Jump to solution
1,286 Views
ganeshh
Contributor III

Hi,

I am planning to buy MCIMX28EVKJ: i.MX28 Evaluation Kit. in hardware schematics SDIO pins are shown but in evaluation kit no headers are given so is it just the sd card slot or pins available . i want to interface a wifi module so sdio pins are needed.

Labels (2)
0 Kudos
Reply
1 Solution
1,163 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ganesh, i.MX28 EVK schematic p.8 shows

SD interface. SDIO interface uses the same pins, i.MX28

has SSP module and it is used for both SD/SDIO.

Actually there is no difference between SD and SDIO signals.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,164 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ganesh, i.MX28 EVK schematic p.8 shows

SD interface. SDIO interface uses the same pins, i.MX28

has SSP module and it is used for both SD/SDIO.

Actually there is no difference between SD and SDIO signals.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply