Accessing OCOTP fuses in linux-fslc 4.1.7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Accessing OCOTP fuses in linux-fslc 4.1.7

706件の閲覧回数
spacemanspiff
Contributor II

Hi all,

I need access to the OCOTP-fuses of i.MX6 from Linux. Read access is currently sufficient.

I see that read support is in the 4.4 and 4.6 branches of linux-fslc, but I had no success porting it to our 4.1.7 tree.

I also tried to include the fsl_otp driver from wandboard-linux (linux-imx-wandboard/fsl_otp.c at master · wolfgar/linux-imx-wandboard · GitHub ). Since we based our board on the wandboard, we originally had this enabled, but now it is not there when we need it.

Are there other options for reading the fuses from Linux?

Does anyone have a patch that applies on 4.1.7? Since we have a bunch of custom patches I would prefer to stick with 4.1.7 for now if possible.

Best regards,

Mikkel Holm Olsen

ラベル(4)
0 件の賞賛
1 返信

469件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Mikkel

4.1.7 tree is not supported on nxp linux releases, one can try

to post this on meta-fsl-arm mailing list, so that someone familiar with

wandboard could try to assist you.

https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛