Accessing OCOTP fuses in linux-fslc 4.1.7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Accessing OCOTP fuses in linux-fslc 4.1.7

671 Views
spacemanspiff
Contributor II

Hi all,

I need access to the OCOTP-fuses of i.MX6 from Linux. Read access is currently sufficient.

I see that read support is in the 4.4 and 4.6 branches of linux-fslc, but I had no success porting it to our 4.1.7 tree.

I also tried to include the fsl_otp driver from wandboard-linux (linux-imx-wandboard/fsl_otp.c at master · wolfgar/linux-imx-wandboard · GitHub ). Since we based our board on the wandboard, we originally had this enabled, but now it is not there when we need it.

Are there other options for reading the fuses from Linux?

Does anyone have a patch that applies on 4.1.7? Since we have a bunch of custom patches I would prefer to stick with 4.1.7 for now if possible.

Best regards,

Mikkel Holm Olsen

Labels (4)
0 Kudos
1 Reply

434 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mikkel

4.1.7 tree is not supported on nxp linux releases, one can try

to post this on meta-fsl-arm mailing list, so that someone familiar with

wandboard could try to assist you.

https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos