Accelerated dual display X11 on imx6 in the future?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Accelerated dual display X11 on imx6 in the future?

1,967 Views
swid
Contributor I

I have been told on the meta-freescale mailinglist, that accelerated, dual-display X11 is not currently possible on the imx6 platform (i.e. using DRI on two displays).

Can someone from freescale confirm this?

I have not found this information in the 'i. MX 6 Graphics User's Guide' or the 'i.MX 6 Linux Reference Manual'.

If I have overlooked it I would appreciate a pointer.

If it is the case, are there plans to implement this?

As I have seen it working with wayland it seems to be technically possible.

Labels (2)
Tags (2)
0 Kudos
Reply
3 Replies

1,534 Views
haggaytavyumi
Contributor III

Hello all

I have the same problem.

I use yocto 3.14.52 BSP with X11.

I have two screens that I have connected to my device.

One through LVDS and one through HDMI.

And I like to run two QT applications on the two screens.

Is it doable?

If not ? Can I modify the driver to support this configuration?

0 Kudos
Reply

1,534 Views
b36401
NXP Employee
NXP Employee

Freescale won't support X11 acceleration for i.MX6x.

Instead, it has support for DirectFB acceleration.

Only i.MX5x has X11 accelerated by hardware (GPU).

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,534 Views
swid
Contributor I

Maybe I asked the wrong question.

I'm not talking about 2d acceleration.

Is it or will it be possible to use glx/egl using DRI on two displays on the i.MX6 platform (concrete i.MX6solo using GC 880 and i.MX6quad using GC 2000)?

0 Kudos
Reply