Hi all,
I want to confirm about Absolute Maximum Ratings for VDD_REG of i.MX53.
My cusoter're using i.MX53.
At our current board, voltage of about 2.6 V is applied due to overshoot at power on, possibly exceeding the operation range of 2.63 V due to ambient environment and part dispersion.
As a phenomenon, we think that there is no problem in operation as long as the margin with the maximum rated range is secured sufficiently due to overshoot before releasing RESET.
Could you tell me the Absolute Maximum Ratings for VDD_REG of i.MX53 ?
Ko-hey
解決済! 解決策の投稿を見る。
Hi Ko-hey
Table 5. Absolute Maximum Ratings i.MX53 datasheet shows
absoulte ratings for some voltages. There is no special VDD_REG data in that table,
so its Absolute Maximum Rating is the same as defined in Table 7. i.MX53xD Operating
Ranges - 2.63V (Max.).
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Ko-hey
Table 5. Absolute Maximum Ratings i.MX53 datasheet shows
absoulte ratings for some voltages. There is no special VDD_REG data in that table,
so its Absolute Maximum Rating is the same as defined in Table 7. i.MX53xD Operating
Ranges - 2.63V (Max.).
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov
Thank you for your quick support.
However, assuming that the operating range = maximum rating, it can be imagined that there is only a margin of 5% and it can not be regarded as the maximum rating.
If it says that there is no regulation, could you confirm whether 10% margin (2.75 V) is OK or NG ?
Ko-hey
Hi Ko-hey
> could you confirm whether 10% margin (2.75 V) is OK or NG ?
not, sorry. Formal answer is:
Table 5. Absolute Maximum Ratings shows parameters which are
characterized on factory. There is no special VDD_REG data in that table,
it was not characterized on factory. So its
Absolute Maximum Rating is the same as defined in
Table 7. i.MX53xD Operating Ranges - 2.63V (Max.).
Best regards
igor