About wifi module issue on imx8mp usdhc1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About wifi module issue on imx8mp usdhc1

715件の閲覧回数
dskim2
Contributor IV

Hi

I am wifi testing with my custorm board.

wifi module is connected to usdhc1 and using 1.8V.

but the information is not correct please see below.

 

root@imx8mp-lpddr4-evk:~#  cat /sys/kernel/debug/mmc1/ios

clock:0 Hz

vdd:0 (invalid)

bus mode:2 (push-pull)

chip select:0 (don't care)

power mode:0 (off)

bus width:0 (1 bits)

timing spec:0 (legacy)

signal voltage:0 (3.30 V)

driver type:0 (driver type B)

yocto version is 6.1.22_2.0.0 and dtb file is imx8mp-evk-usdhc1-m2

 

how can fix it

 

Best Regards

 

 

0 件の賞賛
返信
1 返信

689件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/arch/arm64/boot/dts/freescale/imx8mp-evk-usdhc1-m...

As you can see the regulator voltage is 3.3V, you could change it to 1.8V.

 

0 件の賞賛
返信