About unintentional voltage application before powered on the i.MX6DQ.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About unintentional voltage application before powered on the i.MX6DQ.

ソリューションへジャンプ
1,461件の閲覧回数
keitanagashima
Senior Contributor I

Dear All,

Hello.

The below voltage may occur to the I2C SDA line by external connected device before powered on the i.MX6DQ.

Voltage : 2.0V

Apply Time : 20us

(Board : Custom board)

In this case, is there possibility to destroy i.MX6DQ?

We hope that i.MX6 has the overvoltage protection.

(If it is possible, how many voltage is it possible to endure in i.MX6?)

Best Regards,

Keita

ラベル(2)
0 件の賞賛
返信
1 解決策
1,337件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

[Q1]

> Since as you mention the i.MX6 has overvoltage protection.

Is the overvoltage protection included in i.MX6 all pins with "GPIO" type?

ANSWER: Yes, all the GPIO Type Pads had an overvoltage protection

[Q2]

Is there limitation on the time of voltage applied?

ANSWER. Yes there are but the value it is not available in our datasheet, so it is not validated, I apologize for the inconvenience.

[Q3]

> but in this case it is clearly less than the 3.3v that supports this pad.

Does i.MX6 have the margin to 3.3V limitation?

Is it OK the unintentional voltage less than 3.6 V (= Absolute Maximum Ratings)?

ANSWER.  If you we are talking about the I2C pad, it is different from the GPIO pad, nevertheless it is in the same pin, so I do not see any problem applying the 2.0v for 20ms


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,337件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Keita,

We do not see a problem of the i.Mx6DQ get destroy for applying this 2.0v  for 20ms to the board.  Since as you mention the i.MX6 has overvoltage protection.  I do not have the parameter of how much it is the maxim to allow but in this case it is cleary less than the 3.3v that supports this pad.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,337件の閲覧回数
keitanagashima
Senior Contributor I

Hi jamesbone,

Hello. Sorry, I have additional questions.

[Q1]

> Since as you mention the i.MX6 has overvoltage protection.

Is the overvoltage protection included in i.MX6 all pins with "GPIO" type?

[Q2]

Is there limitation on the time of voltage applied?

[Q3]

> but in this case it is clearly less than the 3.3v that supports this pad.

Does i.MX6 have the margin to 3.3V limitation?

Is it OK the unintentional voltage less than 3.6 V (= Absolute Maximum Ratings)?

Best Regards,

Keita

0 件の賞賛
返信
1,338件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

[Q1]

> Since as you mention the i.MX6 has overvoltage protection.

Is the overvoltage protection included in i.MX6 all pins with "GPIO" type?

ANSWER: Yes, all the GPIO Type Pads had an overvoltage protection

[Q2]

Is there limitation on the time of voltage applied?

ANSWER. Yes there are but the value it is not available in our datasheet, so it is not validated, I apologize for the inconvenience.

[Q3]

> but in this case it is clearly less than the 3.3v that supports this pad.

Does i.MX6 have the margin to 3.3V limitation?

Is it OK the unintentional voltage less than 3.6 V (= Absolute Maximum Ratings)?

ANSWER.  If you we are talking about the I2C pad, it is different from the GPIO pad, nevertheless it is in the same pin, so I do not see any problem applying the 2.0v for 20ms


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,337件の閲覧回数
keitanagashima
Senior Contributor I

Hi Jaime,

Thank you for your reply.

OK. Thank you.

Best Regards,

Keita

0 件の賞賛
返信