About u-boot for UHS-I mode in i.MX6DQ.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About u-boot for UHS-I mode in i.MX6DQ.

732 Views
keitanagashima
Senior Contributor I

Dear All,

Do you have a u-boot which supported UHS-I mode in i.MX6DQ?

We confirmed the Linux kernel was supported UHS-I mode in android L5.0.0_1.0.0.

(UHS-I [SDR104]: 1.8V signaling, Frequency up to 208 MHz, up to 104MB/sec)

But, u-boot wasn't supported it.

(i.e. High Speed mode: 3.3V signaling, Frequency up to 50 MHz, up to 25 MB/sec)

Best Regards,

Keita

0 Kudos
Reply
0 Replies