About to the input timing of the camera signal of i.MX6Solo.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About to the input timing of the camera signal of i.MX6Solo.

跳至解决方案
1,518 次查看
takashitakahash
Contributor III

Dear community.

Our customer has question below.

About  to the input timing of the camera signal of i.MX6Solo, so  should the data be settled at the IP 2 (setup time)?
Or does the data need to be settled before IP
IMX6AEC 4.11.10.3.png

Thank you ,

Best.

takashi.

标签 (1)
0 项奖励
回复
1 解答
1,438 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

>About  to the input timing of the camera signal of i.MX6Solo, so  should the

>data be settled at the IP 2 (setup time)?

yes this is correct understanding

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,439 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

>About  to the input timing of the camera signal of i.MX6Solo, so  should the

>data be settled at the IP 2 (setup time)?

yes this is correct understanding

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复