About to the input timing of the camera signal of i.MX6Solo.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About to the input timing of the camera signal of i.MX6Solo.

Jump to solution
795 Views
takashitakahash
Contributor III

Dear community.

Our customer has question below.

About  to the input timing of the camera signal of i.MX6Solo, so  should the data be settled at the IP 2 (setup time)?
Or does the data need to be settled before IP
IMX6AEC 4.11.10.3.png

Thank you ,

Best.

takashi.

Labels (1)
0 Kudos
1 Solution
715 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

>About  to the input timing of the camera signal of i.MX6Solo, so  should the

>data be settled at the IP 2 (setup time)?

yes this is correct understanding

Best regards
igor
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
716 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

>About  to the input timing of the camera signal of i.MX6Solo, so  should the

>data be settled at the IP 2 (setup time)?

yes this is correct understanding

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos