About to the input timing of the camera signal of i.MX6Solo.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About to the input timing of the camera signal of i.MX6Solo.

ソリューションへジャンプ
1,517件の閲覧回数
takashitakahash
Contributor III

Dear community.

Our customer has question below.

About  to the input timing of the camera signal of i.MX6Solo, so  should the data be settled at the IP 2 (setup time)?
Or does the data need to be settled before IP
IMX6AEC 4.11.10.3.png

Thank you ,

Best.

takashi.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,437件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

>About  to the input timing of the camera signal of i.MX6Solo, so  should the

>data be settled at the IP 2 (setup time)?

yes this is correct understanding

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,438件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

>About  to the input timing of the camera signal of i.MX6Solo, so  should the

>data be settled at the IP 2 (setup time)?

yes this is correct understanding

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信