About the usage of the eMMC device which does not support SPI mode with i.MX6Quad

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

About the usage of the eMMC device which does not support SPI mode with i.MX6Quad

1,131 次查看
yuuki
Senior Contributor II

Dear all,

We use i.MX6Quad.
We want to use eMMC(JEDEC4.51)device.
And we use eMMC Boot.

However, this eMMC does not support SPI mode.
Can we use this eMMC device?

For the method that eMMC(JEDEC4.51) is used in as 4.x,
I referred to the following URL.

https://community.freescale.com/message/435796#435796

However, We do not know whether we can use eMMC which does not support SPI mode.

If we can use this, can MFG tool write a program in this eMMC?

May I have advice?

Best Regards,
Yuuki

标签 (1)
0 项奖励
回复
1 回复

897 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   Basically the SPI mode is not needed for eMMC operation with i.MX6.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复