About the usage of the eMMC device which does not support SPI mode with i.MX6Quad

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About the usage of the eMMC device which does not support SPI mode with i.MX6Quad

1,244件の閲覧回数
yuuki
Senior Contributor II

Dear all,

We use i.MX6Quad.
We want to use eMMC(JEDEC4.51)device.
And we use eMMC Boot.

However, this eMMC does not support SPI mode.
Can we use this eMMC device?

For the method that eMMC(JEDEC4.51) is used in as 4.x,
I referred to the following URL.

https://community.freescale.com/message/435796#435796

However, We do not know whether we can use eMMC which does not support SPI mode.

If we can use this, can MFG tool write a program in this eMMC?

May I have advice?

Best Regards,
Yuuki

ラベル(1)
0 件の賞賛
返信
1 返信

1,010件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   Basically the SPI mode is not needed for eMMC operation with i.MX6.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信