About the spec. of a crystal oscillator required for iMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the spec. of a crystal oscillator required for iMX6

Jump to solution
1,642 Views
yuuki
Senior Contributor II

Dear all,

Would you teach the spec. of the crystal oscillator(32KHz and 24MHz) which i.MX6 needs?

For 24MHz xtal,
I referred to the following URL.
https://community.freescale.com/message/337037#337037

Here, it argues about CL, ESR, etc.


However, It does not argue about the following spec.
- Tolerance
- Temperature Stability
- Operating Temperature

Would you teach about such spec.?

For 32KHz xtal,
I was not able to find the spec. about a 32-kHz crystal oscillator.
Would you teach about the above-mentioned spec.?

May I have advice?

Best Regards,

Labels (1)
0 Kudos
1 Solution
1,087 Views
igorpadykov
NXP Employee
NXP Employee

Hi yuuki

had you looked at IMX6DQ6SDLHDG

Table 2-20. 24 MHz crystal tolerance guidelines  ?

It is named as "24 MHz crystal" - so these tolerances are

for "crystal oscillator connected to XTALI and XTALO".

So if you are using Ethernet - then for it 50ppm  - 24 MHz oscillator tolerance.

Best regards

chip

View solution in original post

0 Kudos
3 Replies
1,087 Views
igorpadykov
NXP Employee
NXP Employee

Hi yuuki

summary (Tolerance +  - Temperature Stability) are defined

in sect.2.7 "Oscillator tolerance"

IMX6DQ6SDLHDG  IMX6DQ6SDLHDG, Hardware Development Guide

For 32KHz there are no such strict requirements, one can follow

for example Table 9 "Recommended External Crystal Specifications"

IMX25AEC i.MX25 Datasheet

Operating Temperature is defined by final product specifications.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,087 Views
yuuki
Senior Contributor II

Dear Chipexpert-san,

Thank you for your support.

For 24MHz,
I referred to IMX6DQ6SDLHDG.
However, I was not able to find the description about the crystal oscillator connected to XTALI and XTALO of iMX6.
Can Tolerance=+-500ppm be used for XTALI and XTALO of iMX6?

Or, Is it necessary to fill the spec. indicated to Table9 of IMX25AEC?


Best Regards,

0 Kudos
1,088 Views
igorpadykov
NXP Employee
NXP Employee

Hi yuuki

had you looked at IMX6DQ6SDLHDG

Table 2-20. 24 MHz crystal tolerance guidelines  ?

It is named as "24 MHz crystal" - so these tolerances are

for "crystal oscillator connected to XTALI and XTALO".

So if you are using Ethernet - then for it 50ppm  - 24 MHz oscillator tolerance.

Best regards

chip

0 Kudos