Hi,
I'm working on a i.mx6q board with LTIB-3.0.35_4.1.0.
When I cross-compile the GDAL,there is a error like below:
/bin/sh /home/myzr/GIS/gdal-1.7.1/libtool --mode=link /opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-fsl-linux-gnueabi-g++ -Wl,-O1 -Wl,-rpath,/usr/local/lib/ -L/usr/local/lib -lgeos_c -lm -lrt -ldl -o libgdal.la /home/myzr/GIS/gdal-1.7.1/frmts/o/*.lo /home/myzr/GIS/gdal-1.7.1/gcore/*.lo /home/myzr/GIS/gdal-1.7.1/port/*.lo /home/myzr/GIS/gdal-1.7.1/alg/*.lo /home/myzr/GIS/gdal-1.7.1/ogr/ogrsf_frmts/o/*.lo ./ogr/ogrgeometryfactory.lo ./ogr/ogrpoint.lo ./ogr/ogrcurve.lo ./ogr/ogrlinestring.lo ./ogr/ogrlinearring.lo ./ogr/ogrpolygon.lo ./ogr/ogrutils.lo ./ogr/ogrgeometry.lo ./ogr/ogrgeometrycollection.lo ./ogr/ogrmultipolygon.lo ./ogr/ogrsurface.lo ./ogr/ogrmultipoint.lo ./ogr/ogrmultilinestring.lo ./ogr/ogr_api.lo ./ogr/ogrfeature.lo ./ogr/ogrfeaturedefn.lo ./ogr/ogrfeaturequery.lo ./ogr/ogrfeaturestyle.lo ./ogr/ogrfielddefn.lo ./ogr/ogrspatialreference.lo ./ogr/ogr_srsnode.lo ./ogr/ogr_srs_proj4.lo ./ogr/ogr_fromepsg.lo ./ogr/ogrct.lo ./ogr/ogr_opt.lo ./ogr/ogr_srs_esri.lo ./ogr/ogr_srs_pci.lo ./ogr/ogr_srs_usgs.lo ./ogr/ogr_srs_dict.lo ./ogr/ogr_srs_panorama.lo ./ogr/ogr_srs_ozi.lo ./ogr/ogr_srs_erm.lo ./ogr/swq.lo ./ogr/ogr_srs_validate.lo ./ogr/ogr_srs_xml.lo ./ogr/ograssemblepolygon.lo ./ogr/ogr2gmlgeometry.lo ./ogr/gml2ogrgeometry.lo ./ogr/ogr_expat.lo \
-rpath /usr/local/lib \
-no-undefined \
-version-info 15:1:14
/bin/grep: /work/fsl-linaro-toolchain-2.13/arm-fsl-linux-gnueabi/lib/default/libstdc++.la: No such file or directory
/bin/sed: can't read /work/fsl-linaro-toolchain-2.13/arm-fsl-linux-gnueabi/lib/default/libstdc++.la: No such file or directory
libtool: link: `/work/fsl-linaro-toolchain-2.13/arm-fsl-linux-gnueabi/lib/default/libstdc++.la' is not a valid libtool archive
make[1]: *** [libgdal.la] Error 1
make[1]: Leaving directory `/home/myzr/GIS/gdal-1.7.1'
make: *** [check-lib] Error 2
I open the the file of libstdc++.la,the last line is:
libdir='/work/fsl-linaro-toolchain-2.13/arm-fsl-linux-gnueabi/lib/default'
But there is no path 'work' in my computer,what should I do?
Solved! Go to Solution.
Thanks for your reply.
When I cross-compiled the gdal-1.7.1 with proj-4.8.0 and geos-3.2.2.
I still meet this error.
So I have to do something for this error.
1.Locate all the libstdc++.la files,and modify these files one by one.I replace the parameter of "libdir" with the path where the libstdc++.la file is.
2.I make the path "/work/fsl-linaro-toolchain-2.13/arm-fsl-linux-gnueabi/lib/default/",and copy one libstdc++.la to the path.
Then I rebuild dal-1.7.1
It works well.
I just tried to use the LTIB to build the gdal without error. Please let me know if you still meet the error when you build it.
Thanks for your reply.
When I cross-compiled the gdal-1.7.1 with proj-4.8.0 and geos-3.2.2.
I still meet this error.
So I have to do something for this error.
1.Locate all the libstdc++.la files,and modify these files one by one.I replace the parameter of "libdir" with the path where the libstdc++.la file is.
2.I make the path "/work/fsl-linaro-toolchain-2.13/arm-fsl-linux-gnueabi/lib/default/",and copy one libstdc++.la to the path.
Then I rebuild dal-1.7.1
It works well.
If you installed the LTIB-3.0.35_4.1.0, the toolchain can be found in the /opt/freescale/usr/local/.
Thanks for your reply.
I have installed the LTIB-3.0.35_4.1.0.
I have succeeded in cross-compiling some projects,such as proj-4.8.0.
The toolchain is in /opt/freescale/usr/local/.