About the process of ISP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

About the process of ISP

1,859 次查看
lei11
Contributor I

The development board I am using is imx8mp, and the SDK version is 6.1.22+g66e442bc7fdc.

I switched the device tree to imx8mp evk dual os08a20. dtb

When I don't do anything, that is to let the system automatically mount. ko ,can generate this data format

lei11_0-1701745006116.png

But when I want to load ko myself

root@imx8mpevk:~# insmod vvcam-dwe.ko
root@imx8mpevk:~# insmod vvcam-isp.ko
root@imx8mpevk:~# insmod imx8-media-dev.ko
root@imx8mpevk:~# insmod os08a20.ko
root@imx8mpevk:~# insmod vvcam-video.ko

 There can only be these three

lei11_2-1701745202856.png

May I ask if there is any operation I missed

0 项奖励
回复
6 回复数

1,819 次查看
lei11
Contributor I
May I ask if anyone can help me ?
0 项奖励
回复

1,811 次查看
joanxie
NXP TechSupport
NXP TechSupport

use command like ./isp_media_server CAMERA0 & to start ISP then check again

0 项奖励
回复

1,753 次查看
lei11
Contributor I


Alternatively, you can provide a complete operation tutorial, such as downloading the 6.1.22+g66e442bc7fdc image from the official website and successfully burning it, as well as how to manually load KO, start ISP, and achieve the same effect as self starting




My current confusion may be that I don't know what series of operations are needed to achieve the same effect as self starting


0 项奖励
回复

1,789 次查看
lei11
Contributor I

lei11_0-1702459657591.png

It's blocking here

0 项奖励
回复

1,797 次查看
lei11
Contributor I

 

lei11_0-1702458110232.png

I executed the command, but only printed this one

 

lei11_1-1702458199378.png

 

0 项奖励
回复

1,740 次查看
joanxie
NXP TechSupport
NXP TechSupport

give me full log for the ./isp_media_server CAMERA0 & to start ISP , I found you have many error on it, and for ISP document, you can find them from nxp official website, we have been released many documents for this, for os08a20, you can refer to the document

https://www.nxp.com.cn/docs/en/application-note/AN13712.pdf

for more detailed document for ISP or other camera, you can find documents from

https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

 

0 项奖励
回复