Hello,
I have two questions.
No1
There is a Hold Delay in the Table.
Does the combination in Description enable the quarter cycle Delay in DDR mode?
No2
QuadSPIx_FLSHCR on 10.2.14.3 has a TDH setting.
Are this setting and Hold Delay in Table 6-50 the same setting?
best regards
Goto
已解决! 转到解答。
@goto11
Hello,
Yes, recommended QuadSPIx_FLSHCR [TDH] settings [should be set to 01
in DDR mode (DDR_EN=1) and set to 00 in SDR mode (DDR_EN=0)] corresponds
QuadSPI configuration boot parameter Hold Delay.
Regards,
Yuri.
@goto11
Hello,
Yes, recommended QuadSPIx_FLSHCR [TDH] settings [should be set to 01
in DDR mode (DDR_EN=1) and set to 00 in SDR mode (DDR_EN=0)] corresponds
QuadSPI configuration boot parameter Hold Delay.
Regards,
Yuri.