About the memory configuration of MX8QM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About the memory configuration of MX8QM

ソリューションへジャンプ
3,093件の閲覧回数
okamotosatoshi
Contributor IV

Hi There,

I am designing a custom board using MX8QM.
The evaluation board uses 32Gbit memory.

MCIMX8QM-CPU MEK Platform - i.MX 8QM CPU CARD
LPDDR4 SDRAM:MT53E768M32D4DT-053 AIT:E
(dual-channel, dual-rank, 32-bit devices)

The 24Gb product is for specific applications and the distribution volume is low, so we are planning to change the parts.
We plan to use dual-channel, single-rank, 32-bit devices.
I believe that the circuit can be configured by simply removing CS1.
Are there any restrictions when using a single rank device?

The adopted chip is “MT53E512M32D1ZW-046BAAT:B”.

Best regards
- satoshi

0 件の賞賛
返信
1 解決策
3,004件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
6 返答(返信)
3,073件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

pls refer to the enclosed files which is for imx8qxp, also can refer to the link as below

"https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8-8X-8XLite-LPDDR4-and-DDR3L-memory...

for HW review, pls create a new ticket for it

0 件の賞賛
返信
3,069件の閲覧回数
okamotosatoshi
Contributor IV

Hi Joanxie,

Thank you for the immediate reply.

We use MX8QM (Quad Max).
Do you have any information on MX8QM (Quad Max)?

I would also appreciate any advice regarding single rank connections!

Best regards
- satoshi

0 件の賞賛
返信
3,051件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

if you use single rank, just use CKE0, CS0. for RPA settings, you can refer to the enclosed file I sent to you

0 件の賞賛
返信
3,033件の閲覧回数
okamotosatoshi
Contributor IV

Hi Joanxie,

Thank you for your advice !

As you pointed out, in addition to CS1, CKE1 is also unnecessary.
It seems that terminal processing of ZQ1 will no longer be necessary.
Single rank uses only CS0, CKE1, and ZQ0.

Additionally, RPA has a cell that selects the SoC.
The following items can be selected.

・MX8 QuadXPlus and DualXPlus
・MX8 DualX

Which is the correct choice for MX8QM (Quad Max) ?

Best regards
- satoshi

0 件の賞賛
返信
3,005件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
2,987件の閲覧回数
okamotosatoshi
Contributor IV

Hi Joanxie,

Now that we have collected hardware and software information, we can proceed with development.
Thank you for your support.

Best regards
- satoshi

0 件の賞賛
返信